Silicon Labs
gecko-os/4/standard/latest/group-api-dms-macros
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
    Results 1-5 of 5 for gecko-os/4/standard/latest/group-api-dms-macros in 0.18 seconds
    Commands - v4.1 - Gecko OS API Documentation Silicon Labs
    https://docs.silabs.com/.../group-api-core-comm...
    Issue Gecko OS command, return the uint32 result. ... Issue Gecko OS command, store string result in buffer. ... ) Issue Gecko OS Command. For available commands, see Gecko OS Command API .
    ProductWireless Resource TypeSoftware API documentation
    Gecko OS 4.2 Command API Silicon Labs
    https://docs.silabs.com/.../...
    Gecko OS 4.2 Command API The Command API documentation provides details of commands and variables as well as lots of Command API examples covering a wide range of uses.
    Update and Recovery - v4.1 - Gecko OS API Documentation Silicon Labs
    https://docs.silabs.com/.../update-and-recov...
    Gecko OS is part of a larger sophisticated application framework installed on all Gecko OS devices. ... dms_claim <dms_token> The Gecko DMS Commands When using Gecko OS, DMS commands is ... ls
    ProductWireless Resource TypeSoftware API documentation
    BGX13-1.x Command Reference - v1.0 - Gecko OS API Documentation Silicon Labs
    https://docs.silabs.com/.../comma...
    ... page provides a list of Bluetooth Xpress API commands with a full description of how ... os pins can only use the strong drive strength. ... Output, open-source with pull-up (see gdi os pren )
    ProductWireless Resource TypeSoftware API documentation
    Gecko OS Commands Silicon Labs
    https://docs.silabs.com/.../comma...
    The Gecko OS Command API is friendly for humans too. ... dms_activate <product code> [ update /-o / -m] ... Gecko OS writes the file to extended flash or bulk flash, depending on the location ...
      Results 1-5 of 5 for gecko-os/4/standard/latest/group-api-dms-macros