Issue Gecko OS command, return the uint32 result. ... Issue Gecko OS command, store string result in buffer. ... ) Issue Gecko OS Command. For available commands, see Gecko OS Command API .
ProductWirelessResource TypeSoftware API documentation
Gecko OS 4.2 Command API The Command API documentation provides details of commands and variables as well as lots of Command API examples covering a wide range of uses.
Gecko OS is part of a larger sophisticated application framework installed on all Gecko OS devices. ... See Device Firmware Update . The Device Management Server (DMS) To update a Gecko OS ...
ProductWirelessResource TypeSoftware API documentation
... application (e.g., putting them below FreeRTOS OS atomic for access to OS functions in RAIL callbacks). ... This API indicates that the DCDC peripheral bus clock has changed allowing RAIL to ...
os pins can only use the strong drive strength. ... Output, open-source with pull-up (see gdi os pren ) ... stream mode, either with the str_select GPIO (see gfu ), or by issuing the the str ...
ProductWirelessResource TypeSoftware API documentation
Results 1-5 of 5 for gecko-os/4/standard/latest/group-api-proto-http-server-stream-ws-api