Gecko OS is part of a larger sophisticated application framework installed on all Gecko OS devices. ... The Gecko OS Device Firmware Update (DFU) feature allows device firmware to be updated ...
ProductWirelessResource TypeSoftware API documentation
Commands Core Functions for issuing Gecko OS commands. More. ... ) Issue Gecko OS Command. For available commands, see Gecko OS Command API . ... fmt Formatted Gecko OS serial command Returns
ProductWirelessResource TypeSoftware API documentation
Gecko OS 4.2 Command API The Command API documentation provides details of commands and variables as well as lots of Command API examples covering a wide range of uses.
Gecko OS evaluation boards are by default configured to enter Setup Web mode when you hold down Button 2 ... As well as standard Gecko OS terminal behavior, the Console tab provides additional ...
... page provides a list of Bluetooth Xpress API commands with a full description of how ... os pins can only use the strong drive strength. ... Output, open-source with pull-up (see gdi os pren )
ProductWirelessResource TypeSoftware API documentation
Results 1-5 of 5 for gecko-os/4/standard/latest/group-api-rtos