Issue Gecko OS command, return the uint32 result. ... Issue Gecko OS command, store string result in buffer. ... ) Issue Gecko OS Command. For available commands, see Gecko OS Command API .
ProductWirelessResource TypeSoftware API documentation
Gecko OS 4.2 Command API The Command API documentation provides details of commands and variables as well as lots of Command API examples covering a wide range of uses.
Gecko OS is part of a larger sophisticated application framework installed on all Gecko OS devices. ... If system.safemode.ota_auto_retry is enabled, the safemode app repeatedly attempts OTA.
ProductWirelessResource TypeSoftware API documentation
Example Example usage. Alphabetical List of Commands ... os pins can only use the strong drive strength. ... Returns the RSSI value from the latest received packet of the current active ...
ProductWirelessResource TypeSoftware API documentation
This document describes using the Flex SDK for 802.15.4 development on EFR32™ Wireless parts. ... 4.1 Applying a PHY from RAIL rx 0 // Configs can be loaded only in radio Idle state ...
Resource TypeApplication Notes
Results 1-5 of 5 for gecko-os/4/standard/latest/group-api-sdk-example-app-util