Silicon Labs
gecko-os/4/standard/latest/group-api-settings
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
    Results 1-5 of 5 for gecko-os/4/standard/latest/group-api-settings in 0.05 seconds
    Update and Recovery - v4.1 - Gecko OS API Documentation Silicon Labs
    https://docs.silabs.com/.../update-and-recov...
    Gecko OS is part of a larger sophisticated application framework installed on all Gecko OS devices. ... 0 = no, 1 = yes <- Print a list of faults (8 faults should print) <- Reset faults ... ls
    ProductWireless Resource TypeSoftware API documentation
    Gecko OS 4.2 Command API Silicon Labs
    https://docs.silabs.com/.../...
    Gecko OS 4.2 Command API The Command API documentation provides details of commands and variables as well as ... Overview for a description of the general structure and features of Gecko OS 4.
    Commands - v4.1 - Gecko OS API Documentation Silicon Labs
    https://docs.silabs.com/.../group-api-core-comm...
    Issue Gecko OS command, store string result in buffer. ... fmt Formatted Gecko OS serial command Returns ... will execute in the Command thread context, the supplied callback is invoked after ...
    ProductWireless Resource TypeSoftware API documentation
    Gecko OS Commands Silicon Labs
    https://docs.silabs.com/.../comma...
    ... , file version defaults to 1.0.0 . -t <type> t ype: specify file type as integer or hex string 2 . ... 1 : Some options can be combined with a single dash, e.g. -de , -eu , or supplied as ...
    BGX13-1.x Command Reference - v1.0 - Gecko OS API Documentation Silicon Labs
    https://docs.silabs.com/.../comma...
    BGX13-1.x Command Reference This page provides a list of Bluetooth Xpress API commands with a full description of ... os pins can only use the strong drive strength. ... > gge 5 1 gges
    ProductWireless Resource TypeSoftware API documentation
      Results 1-5 of 5 for gecko-os/4/standard/latest/group-api-settings