Gecko OS is part of a larger sophisticated application framework installed on all Gecko OS devices. ... The Gecko OS Device Firmware Update (DFU) feature allows device firmware to be updated ...
ProductWirelessResource TypeSoftware API documentation
Gecko OS 4.2 Command API The Command API documentation provides details of commands and variables as well as lots of Command API examples covering a wide range of uses.
Modules ... [out] buffer Buffer to hold returned data [in] ... [out] buffer Buffer to hold string result [in] ... Issue Gecko OS command asynchronously and invoke callback on completion.
ProductWirelessResource TypeSoftware API documentation
... page provides a list of Bluetooth Xpress API commands with a full description of how ... os pins can only use the strong drive strength. ... Output, open-source with pull-up (see gdi os pren )
ProductWirelessResource TypeSoftware API documentation
Dynamic FEC configuration is supported on SUN FSK PHYs only. ... 4.3.1 Enable Address Filtering HW accelerated MAC features, such as frame and address ... | | 4.5 Long Address Example
Resource TypeApplication Notes
Results 1-5 of 5 for gecko-os/4/standard/latest/group-api-settings-gos-macros