Silicon Labs
gecko-os/4/standard/latest/group-api-system-indicator
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
Results 1-5 of 5 for gecko-os/4/standard/latest/group-api-system-indicator in 0.18 seconds
Gecko OS 4.2 Command API Silicon Labs
https://docs.silabs.com/.../...
Gecko OS 4.2 Command API The Command API documentation provides details of commands and variables as well as ... Overview for a description of the general structure and features of Gecko OS 4.
Update and Recovery - v4.1 - Gecko OS API Documentation Silicon Labs
https://docs.silabs.com/.../update-and-recov...
Gecko OS is part of a larger sophisticated application framework installed on all Gecko OS devices. ... format_flash get ls ... get wlan.mac to obtain the device MAC address
ProductWireless Resource TypeSoftware API documentation
Commands - v4.1 - Gecko OS API Documentation Silicon Labs
https://docs.silabs.com/.../group-api-core-comm...
Issue Gecko OS command, store string result in buffer. ... Issue Gecko OS command, return result data in buffer. ... Examples: network/ethernet_bridge/main.c . ◆ gos_cmd_issue_with_data()
ProductWireless Resource TypeSoftware API documentation
BGX13-1.x Command Reference - v1.0 - Gecko OS API Documentation Silicon Labs
https://docs.silabs.com/.../comma...
os pins can only use the strong drive strength. ... Get the current value of a general purpose I/O pin configured for the stdio function. ... Get a list of values for all GPIOs at once.
ProductWireless Resource TypeSoftware API documentation
UG489: Silicon Labs Gecko Bootloader User's Guide for GSDK 4.0 and Higher
https://www.silabs.com/.../ug489-gecko-bootloader-user-guide-gsdk-4....
. 20 4.1.1 4.1.2 4.1.3 ... 1. SPI Flash Storage: The SPI flash storage implementation supports a variety of SPI ... Gecko Bootloader has been built using GSDK v4.0, it is recommended that the ...
Resource TypeUser's Guides
    Results 1-5 of 5 for gecko-os/4/standard/latest/group-api-system-indicator