Gecko OS 4.2 Command API The Command API documentation provides details of commands and variables as well as lots of Command ... Commands Variables Examples
gos_result_t gos_cmd_issue (const char *fmt,.) Issue Gecko OS Command. More. ... Issue Gecko OS command, return the uint32 result. ... Issue Gecko OS command, store string result in buffer.
ProductWirelessResource TypeSoftware API documentation
1 - an update is available, the contains the new bundle version string 2 - no update available (i.e. the device's current firmware is up-to-date) <message ... ipd 1 Input, high-impedance
Gecko OS is part of a larger sophisticated application framework installed on all Gecko OS devices. ... system.cmd.buffered system.cmd.echo system.cmd.header_enabled system.cmd.prompt_enabled
ProductWirelessResource TypeSoftware API documentation
BGX13-1.x Command Reference This page provides a list of Bluetooth Xpress API ... <index> - the index obtained from the scan command output ... os pins can only use the strong drive strength.
ProductWirelessResource TypeSoftware API documentation
Results 1-5 of 5 for gecko-os/4/standard/latest/group-api-system-misc