Gecko OS 4.2 Command API The Command API documentation provides details of commands and variables as well as lots of Command API examples covering a wide range of uses.
Gecko OS is part of a larger sophisticated application framework installed on all Gecko OS devices. ... Safe mode operation is guaranteed in the unlikely event the device is configured in a ...
ProductWirelessResource TypeSoftware API documentation
Issue Gecko OS command, return the uint32 result. ... Issue Gecko OS command, store string result in buffer. ... ) Issue Gecko OS Command. For available commands, see Gecko OS Command API .
ProductWirelessResource TypeSoftware API documentation
This page provides a list of Bluetooth Xpress API commands with a full description of how ... Example usage. Alphabetical List of Commands A ... os pins can only use the strong drive strength.
ProductWirelessResource TypeSoftware API documentation
... the standard PHYs defined by the 802.15.4 PHY layer specification, it is possible to ... 4.1 Applying a PHY from RAIL rx 0 // Configs can be loaded only in radio Idle state config2p4GHz802154 ...
Resource TypeApplication Notes
Results 1-5 of 5 for gecko-os/4/standard/latest/group-api-util-safe-slinked-list-macros