Determine if your Hurricane Board is Running a Leaderboard Demo
You can determine if your Hurricane board is running a Leaderboard Demo by checking the customr code. If the customer code is LEADER
then your device is activated and programmed with a Leaderboard Demo.
Either of the two methods below will help you discover your customer code.
In the Hurricane menu navigate to
System Diagnostics
thenSoftware Information
. The customer code will be listed on this page.In the device console, type the command
version
. The first part in the version string is in the format of:CUSTOMER-PRODUCT-BUNDLE
. If theCUSTOMER
field is LEADER then your device is running a Leaderboard Demo. In the example below the board is running the Leaderboard Weather Demo version 0.0.10.
> version
LEADER-WEATHER-0.0.10, Gecko_OS-STANDARD-4.0.18-1928, WGM160P_BETA