Time
time.last_set
Abbreviation
ti l
Access
get
Description
Return the number of seconds since the time was set or -1
if the time has never been set. Time can be set manually or via NTP.
Arguments
None
Default
None
Platforms
- WGM160P
Gecko OS Plugin
Get example
> get ti l
R000005
239
time.rtc
Abbreviation
ti r
Access
get/set
Description
The local time. Read returns epoch seconds by default, or (optionally) epoch milliseconds or UTC. Write takes an <epoch seconds>
argument.
Get arguments
[ms/utc]
Set arguments
<epoch seconds>
Default
None
Platforms
- WGM160P
Properties
- takes effect immediately
Gecko OS Plugin
Get example
> get ti r utc
R000029
2019-01-01-23T08:13:07.010248Z
Set example
> set ti r 1395562166
R000008
Set OK
time.uptime
Abbreviation
ti u
Access
get
Description
Returns the number of seconds since reset, guaranteed not to roll over in your lifetime!
Arguments
Default
None
Platforms
- WGM160P
Gecko OS Plugin
Get example
> get ti u
R000006
8576
time.zone
Abbreviation
ti z
Access
get/set
Description
Timezone offset from GMT in hours.
Arguments
[+/-]H[:M]
Offset ranges from -12:30
to 12:30
.
where:
H
is an integer between 0 and 12M
(if present) = 30
Default
0
Platforms
- WGM160P
Properties
- takes effect immediately
Gecko OS Plugin
Get example
> get ti z
R000007
-4:30
Set example
> set ti z -4:30
R000008
Set OK