update - optional: invoke a DFU after successful activation ... Gecko OS writes the file to extended flash or bulk flash, depending on the location ... Gecko OS Plugin file_system Examples
Gecko OS 4.2 Command API The Command API documentation provides details of commands and variables as well as lots of Command API examples covering a wide range of uses.
... in the examples on this page were captured with system print level ( sy p ) = all, and system command header enabled ( sy c h ) = true. ... os pins can only use the strong drive strength.
ProductWirelessResource TypeSoftware API documentation
... exposed through the Flex SDK. These release notes cover SDK version(s): Gecko SDK 3.0.0.2 released July 29, 2020 silabs.com | Building a ... Gecko Bootloader Added rollback prevention feature
Resource TypeRelease Notes
Results 1-5 of 5 for gecko-os/4/standard/latest/sdk/api/gos_cmd_update_system_monitor