Gecko OS is part of a larger sophisticated application framework installed on all Gecko OS devices. ... dms_claim <dms_token> The Gecko DMS Commands When using Gecko OS, DMS commands is ...
ProductWirelessResource TypeSoftware API documentation
Gecko OS 4.2 Command API The Command API documentation provides details of commands and variables as well as lots of Command API examples covering a wide range of uses.
os pins can only use the strong drive strength. ... Output, push-pull 4 Output, open-drain with no pull-up (see gdi od prdi ) ... Set the value for all GPIOs at once, using a list of settings.
ProductWirelessResource TypeSoftware API documentation
... that PSA Crypto is the recommended device independent crypto API and should be used whenever possible. ... and software-driven tamper signals to a set of configurable hardware and software ...
Results 1-5 of 5 for gecko-os/4/standard/latest/sdk/api/gos_dms_set_message_fallback_handler