Silicon Labs
gecko-os/4/standard/latest/sdk/api/gos_hs_close_keepalive_connection
Clear
SearchLoading
Explore a fresh approach to searching with our
AI-driven document search.
powered by
  • Docs Home
  • DocSpace
  • Last Page Titlle
  • Docs Search
Relevancy Latest
Filter by:
Filter by:
Filter by:
Narrow By
Collapse All

Software Docs

Loading

Products

Loading

    Resource Type

    Loading

    Language

    Loading
    Clear All Filters

    All Results

    Software Docs

    Products

    Results 1-5 of 5 for gecko-os/4/standard/latest/sdk/api/gos_hs_close_keepalive_connection in 0.30 seconds
    Update and Recovery - v4.1 - Gecko OS API Documentation Silicon Labs
    https://docs.silabs.com/.../update-and-recov...
    Gecko OS is part of a larger sophisticated application framework installed on all Gecko OS devices. ... The Gecko OS Device Firmware Update (DFU) feature allows device firmware to be updated ...
    ProductWireless Resource TypeSoftware API documentation
    Gecko OS 4.2 Command API Silicon Labs
    https://docs.silabs.com/.../...
    Gecko OS 4.2 Command API The Command API documentation provides details of commands and variables as well as lots of Command API examples covering a wide range of uses.
    Commands - v4.1 - Gecko OS API Documentation Silicon Labs
    https://docs.silabs.com/.../group-api-core-comm...
    Functions gos_result_t gos_cmd_issue (const char *fmt,.) Issue Gecko OS Command. More. ... More. gos_result_t gos_cmd_issue_with_data (const void *data, uint16_t length, const char *fmt,.)
    ProductWireless Resource TypeSoftware API documentation
    BGX13-1.x Command Reference - v1.0 - Gecko OS API Documentation Silicon Labs
    https://docs.silabs.com/.../comma...
    ... page provides a list of Bluetooth Xpress API commands with a full description of how ... The device already has a connection to a peripheral ... os pins can only use the strong drive strength.
    ProductWireless Resource TypeSoftware API documentation
    SE Manager | API Documentation | Platform | v5.0.1 | Silicon Labs
    https://docs.silabs.com/.../sl-se-mana...
    ... PSA Crypto is the recommended device independent crypto API and should be used whenever possible. ... the device will erase OTP and become inoperable if 4 glitch signals is seen in a 1 minute ...
      Results 1-5 of 5 for gecko-os/4/standard/latest/sdk/api/gos_hs_close_keepalive_connection