HTTP Server

HTTP server functions. More...

Modules

Types
HTTP server data types.
 
Macros
HTTP server macros.
 

Functions

bool gos_hs_is_running (void)
 Returns if the HTTP server is running. More...
 
char * gos_hs_url_decode (char *buffer)
 Decode URL encoded string destructively (i.e. in-place) More...
 
gos_result_t gos_hs_read_post_data (const gos_hs_request_t *request, gos_buffer_t *buffer, uint32_t timeout_ms)
 Read body of HTTP POST request. More...
 
gos_result_t gos_hs_write_reply_header (const gos_hs_request_t *request, const char *mime_type, int32_t length, gos_hs_response_flag_t flags)
 Return HTTP response with a 200 status code. More...
 
gos_result_t gos_hs_write_reply_header_with_config (const gos_hs_request_t *request, const gos_hs_reply_config_t *config)
 Return HTTP response with specified configuration. More...
 
gos_result_t gos_hs_write_chunked_data (const gos_hs_request_t *request, const void *data, uint32_t data_len, bool flush_now)
 Write HTTP body with chunked encoding. More...
 
gos_result_t gos_hs_write_data (const gos_hs_request_t *request, const void *data, uint32_t data_len, bool flush_now)
 Write HTTP body with non-chunked encoding. More...
 
bool gos_hs_authorize_user (const gos_hs_request_t *request, char *processing_buffer, const char *user, const char *password)
 Authorize HTTP request user credentials. More...
 
gos_result_t gos_hs_write_unauthorized_response (const gos_hs_request_t *request)
 Return Unauthorized HTTP response. More...
 
gos_result_t gos_hs_write_not_found_response (const gos_hs_request_t *request)
 Return Not Found HTTP response. More...
 
gos_result_t gos_hs_return_status_code (const gos_hs_request_t *request, uint32_t code, const char *msg)
 Return HTTP response with status code. More...
 
void gos_hs_register_dynamic_page (const gos_hs_dynamic_page_t *page)
 Register dynamic URL callback. More...
 
void gos_hs_register_header_callback (const gos_hs_custom_header_callback_t callback)
 Register custom header callback. More...
 
void gos_hs_register_authorize_callback (const gos_hs_authorize_callback_t callback)
 Register unauthorized callback. More...
 
void gos_hs_register_not_found_callback (const gos_hs_not_found_callback_t callback)
 Register page not found callback. More...
 
gos_hs_param_tgos_hs_request_get_param (const gos_hs_request_t *request, const char *key)
 Return GET parameter with specified key. More...
 
gos_hs_header_tgos_hs_request_get_header (const gos_hs_request_t *request, const char *key)
 Return request header with specified key. More...
 
gos_hs_method_t gos_hs_request_get_method (const gos_hs_request_t *request)
 Return the method type of the HTTP request. More...
 
int32_t gos_hs_request_get_content_length (const gos_hs_request_t *request)
 Return the number of bytes available from the HTTP request. More...
 
gos_result_t gos_hs_get_tls_client_list (gos_hs_tls_client_t **client_list_ptr)
 Return list of recently connected TLS clients. More...
 
void gos_hs_destroy_tls_client_list (gos_hs_tls_client_t *client_list)
 Release memory allocated by gos_hs_get_tls_client_list() More...
 

Detailed Description

HTTP server functions.

Function Documentation

◆ gos_hs_authorize_user()

bool gos_hs_authorize_user ( const gos_hs_request_t request,
char *  processing_buffer,
const char *  user,
const char *  password 
)

Authorize HTTP request user credentials.

This validates the provided Basic credentials in an HTTP request. More info here

This should be call immediately after a gos_hs_request_processor_t callback. Typically gos_hs_write_unauthorized_response() would be called if this function returns false.

Parameters
requestInternal HTTP request pointer, provided by gos_hs_request_processor_t callback
processing_bufferThis is used for internal prcoessing, it should be at least 64 bytes
userThe user name to validate against, set to NULL to use the http.server.username setting
passwordThe password to validate against, set to NULL to use the http.server.password setting
Returns
gos_result_t result of api call

◆ gos_hs_destroy_tls_client_list()

void gos_hs_destroy_tls_client_list ( gos_hs_tls_client_t client_list)

Release memory allocated by gos_hs_get_tls_client_list()

Parameters
client_listList returned by gos_hs_get_tls_client_list()

◆ gos_hs_get_tls_client_list()

gos_result_t gos_hs_get_tls_client_list ( gos_hs_tls_client_t **  client_list_ptr)

Return list of recently connected TLS clients.

Return list of recently connected clients. Up to 8 clients are logged. When the log contains 8 clients and a new client is added, the oldest client is removed. Requires http.server.tls_log_clients to be enabled.

gos_hs_destroy_tls_client_list() must be called to free the memory allocated by the returned list.

See Gecko OS Command API documentation: http.server.tls_client_log.

Parameters
[out]client_list_ptrPointer to hold linked list of gos_hs_tls_client_t

◆ gos_hs_is_running()

bool gos_hs_is_running ( void  )

Returns if the HTTP server is running.

Returns
true if the HTTP server is running, false else

◆ gos_hs_read_post_data()

gos_result_t gos_hs_read_post_data ( const gos_hs_request_t request,
gos_buffer_t buffer,
uint32_t  timeout_ms 
)

Read body of HTTP POST request.

This should be used in a gos_hs_request_processor_t callback.

Parameters
requestInternal HTTP request pointer, provided by gos_hs_request_processor_t callback
bufferPointer to the gos_buffer_t to be filled with the HTTP post body and number of bytes read
timeout_msStream read timeout in milliseconds
Returns
gos_result_t result of api call
Examples:
network/http_server/requests/json_parser.c.

◆ gos_hs_register_authorize_callback()

void gos_hs_register_authorize_callback ( const gos_hs_authorize_callback_t  callback)

Register unauthorized callback.

Register callback to be called to authorized username/password of HTTP request. The callback executes in the HTTP server thread.

Parameters
callbackCallback to be called before processing HTTP request, see gos_hs_authorize_callback_t
Returns
gos_result_t result of api call

◆ gos_hs_register_dynamic_page()

void gos_hs_register_dynamic_page ( const gos_hs_dynamic_page_t page)

Register dynamic URL callback.

The callback will be called when the specified URL is requested. The callback executes in the HTTP server thread context.

Parameters
pageURL/callback to register, see gos_hs_dynamic_page_t
Returns
gos_result_t result of api call

◆ gos_hs_register_header_callback()

void gos_hs_register_header_callback ( const gos_hs_custom_header_callback_t  callback)

Register custom header callback.

Register callback to be called for each HTTP request header. This allows for storing custom HTTP headers in the HTTP request object.

The custom headers are retrieved from the gos_hs_request_t with gos_hs_request_get_header() The callback executes in the HTTP server thread BEFORE the gos_hs_request_processor_t is called.

Parameters
callbackCallback to be called for each HTTP header, see gos_hs_custom_header_callback_t
Returns
gos_result_t result of api call

◆ gos_hs_register_not_found_callback()

void gos_hs_register_not_found_callback ( const gos_hs_not_found_callback_t  callback)

Register page not found callback.

Register callback to be called if requested URL is not found. The callback executes in the HTTP server thread.

Parameters
callbackCallback to be called if request URL is not found, see gos_hs_not_found_callback_t
Returns
gos_result_t result of api call

◆ gos_hs_request_get_content_length()

int32_t gos_hs_request_get_content_length ( const gos_hs_request_t request)

Return the number of bytes available from the HTTP request.

If the request is chunked encoded then this returns the number of remaining bytes in the current chunk, otherwise this returns the number of bytes in the request body.

Note
This should be used in a gos_hs_request_processor_t callback.
Parameters
requestInternal HTTP request pointer, provided by gos_hs_request_processor_t callback
Returns
Number of bytes available to be read

◆ gos_hs_request_get_header()

gos_hs_header_t* gos_hs_request_get_header ( const gos_hs_request_t request,
const char *  key 
)

Return request header with specified key.

This allows for returning a HTTP header with the given key. Note that only gos_hs_request_header_t are returned with a HTTP request by default. To return custom headers, use gos_hs_register_header_callback() This should be used in a gos_hs_request_processor_t callback.

Parameters
requestInternal HTTP request pointer, provided by gos_hs_request_processor_t callback
keyThe HTTP header's key value
Returns
gos_hs_header_t if header with key found, NULL else

◆ gos_hs_request_get_method()

gos_hs_method_t gos_hs_request_get_method ( const gos_hs_request_t request)

Return the method type of the HTTP request.

This should be used in a gos_hs_request_processor_t callback.

Parameters
requestInternal HTTP request pointer, provided by gos_hs_request_processor_t callback
Returns
The gos_hs_method_t of the current HTTP request
Examples:
network/http_server/requests/json_parser.c.

◆ gos_hs_request_get_param()

gos_hs_param_t* gos_hs_request_get_param ( const gos_hs_request_t request,
const char *  key 
)

Return GET parameter with specified key.

Returns a GET parameter's value.

A GET request contains parameters of the form:

http://mydevice.com/my_dynamic_webpage?param1=123&param2=abc

The get the request's param1, the following code would be used:

gos_hs_param_t *param1 = gos_hs_request_get_param(request, "param1");

This should be used in a gos_hs_request_processor_t callback.

Parameters
requestInternal HTTP request pointer, provided by gos_hs_request_processor_t callback
keyThe parameter's key value
Returns
gos_hs_param_t if key found, NULL else
Examples:
network/http_server/requests/get_params.c.

◆ gos_hs_return_status_code()

gos_result_t gos_hs_return_status_code ( const gos_hs_request_t request,
uint32_t  code,
const char *  msg 
)

Return HTTP response with status code.

Return a HTTP status code with optional message. The message is printed in the body of the response.

More info about HTTP status codes: here

This should be used in a gos_hs_request_processor_t callback.

Note
The HTTP client request is closed after the response is sent.
Parameters
requestInternal HTTP request pointer, provided by gos_hs_request_processor_t callback
codeThe http status code.
msgOptional message to print in body of response
Returns
gos_result_t result of api call
Examples:
network/http_server/requests/get_params.c, network/http_server/requests/json_parser.c, and network/http_server/requests/set_light.c.

◆ gos_hs_url_decode()

char* gos_hs_url_decode ( char *  buffer)

Decode URL encoded string destructively (i.e. in-place)

Parameters
bufferPointer to url encoded string
Returns
Same pointer as buffer, with contents url decoded

◆ gos_hs_write_chunked_data()

gos_result_t gos_hs_write_chunked_data ( const gos_hs_request_t request,
const void *  data,
uint32_t  data_len,
bool  flush_now 
)

Write HTTP body with chunked encoding.

Write the body of a HTTP request using 'Transfer-Encoding: chunked'.

gos_hs_write_reply_header() must be called first with its 'length' parameter set to -1.

This should be used in a gos_hs_request_processor_t callback.

Parameters
requestInternal HTTP request pointer, provided by gos_hs_request_processor_t callback
dataData to write to response
data_lenAmount of data to write
flush_nowSet to false if there is more data to write, true if this is the last write (which will complete the response)
Returns
gos_result_t result of api call
Examples:
network/http_server/requests/json_generator.c.

◆ gos_hs_write_data()

gos_result_t gos_hs_write_data ( const gos_hs_request_t request,
const void *  data,
uint32_t  data_len,
bool  flush_now 
)

Write HTTP body with non-chunked encoding.

Write the body of the HTTP request using 'Content-Legnth: xxx'

gos_hs_write_reply_header() must be called first with its 'length' parameter > 0.

This should be used in a gos_hs_request_processor_t callback.

Parameters
requestInternal HTTP request pointer, provided by gos_hs_request_processor_t callback
dataData to write to response
data_lenAmount of data to write
flush_nowSet to false if there is more data to write, true if this is the last write (which will complete the response)
Returns
gos_result_t result of api call
Examples:
network/http_server/requests/get_params.c, network/http_server/requests/json_parser.c, network/http_server/requests/root_page.c, network/http_server/requests/set_light.c, and network/http_server/requests/toggle_light.c.

◆ gos_hs_write_not_found_response()

gos_result_t gos_hs_write_not_found_response ( const gos_hs_request_t request)

Return Not Found HTTP response.

Return a 404 Not Found HTTP response

This should be used in a gos_hs_request_processor_t callback.

Parameters
requestInternal HTTP request pointer, provided by gos_hs_request_processor_t callback
Returns
gos_result_t result of api call

◆ gos_hs_write_reply_header()

gos_result_t gos_hs_write_reply_header ( const gos_hs_request_t request,
const char *  mime_type,
int32_t  length,
gos_hs_response_flag_t  flags 
)

Return HTTP response with a 200 status code.

Completes a HTTP request with a 200 status code.

This should be used in a gos_hs_request_processor_t callback.

Note
To return a non-200 code, see gos_hs_return_status_code()
Parameters
requestInternal HTTP request pointer, provided by gos_hs_request_processor_t callback
mime_typeThe response 'Content-Type', set NULL if unused
lengthThe 'Content-Length' if > 0, set to -1 for 'Transfer-Encoding: chunked'
flagsOptionals flags to add to the response headers, gos_hs_response_flag_t
Returns
gos_result_t result of api call
Examples:
network/http_server/requests/get_params.c, network/http_server/requests/json_generator.c, network/http_server/requests/json_parser.c, network/http_server/requests/root_page.c, network/http_server/requests/set_light.c, and network/http_server/requests/toggle_light.c.

◆ gos_hs_write_reply_header_with_config()

gos_result_t gos_hs_write_reply_header_with_config ( const gos_hs_request_t request,
const gos_hs_reply_config_t config 
)

Return HTTP response with specified configuration.

Completes a HTTP request with the specified configuration

This should be used in a gos_hs_request_processor_t callback.

Parameters
requestInternal HTTP request pointer, provided by gos_hs_request_processor_t callback
configThe reply configuration, see gos_hs_reply_config_t
Returns
gos_result_t result of api call

◆ gos_hs_write_unauthorized_response()

gos_result_t gos_hs_write_unauthorized_response ( const gos_hs_request_t request)

Return Unauthorized HTTP response.

Return a 403 Unauthorized HTTP response

This should be used in a gos_hs_request_processor_t callback.

Parameters
requestInternal HTTP request pointer, provided by gos_hs_request_processor_t callback
Returns
gos_result_t result of api call