HTTP Server
HTTP server functions. More...
Modules | |
Types | |
HTTP server data types. | |
Macros | |
HTTP server macros. | |
Functions | |
bool | gos_hs_is_running (void) |
Returns if the HTTP server is running. More... | |
char * | gos_hs_url_decode (char *buffer) |
Decode URL encoded string destructively (i.e. in-place) More... | |
gos_result_t | gos_hs_read_post_data (const gos_hs_request_t *request, gos_buffer_t *buffer, uint32_t timeout_ms) |
Read body of HTTP POST request. More... | |
gos_result_t | gos_hs_write_reply_header (const gos_hs_request_t *request, const char *mime_type, int32_t length, gos_hs_response_flag_t flags) |
Return HTTP response with a 200 status code. More... | |
gos_result_t | gos_hs_write_reply_header_with_config (const gos_hs_request_t *request, const gos_hs_reply_config_t *config) |
Return HTTP response with specified configuration. More... | |
gos_result_t | gos_hs_write_chunked_data (const gos_hs_request_t *request, const void *data, uint32_t data_len, bool flush_now) |
Write HTTP body with chunked encoding. More... | |
gos_result_t | gos_hs_write_data (const gos_hs_request_t *request, const void *data, uint32_t data_len, bool flush_now) |
Write HTTP body with non-chunked encoding. More... | |
bool | gos_hs_authorize_user (const gos_hs_request_t *request, char *processing_buffer, const char *user, const char *password) |
Authorize HTTP request user credentials. More... | |
gos_result_t | gos_hs_write_unauthorized_response (const gos_hs_request_t *request) |
Return Unauthorized HTTP response. More... | |
gos_result_t | gos_hs_write_not_found_response (const gos_hs_request_t *request) |
Return Not Found HTTP response. More... | |
gos_result_t | gos_hs_return_status_code (const gos_hs_request_t *request, uint32_t code, const char *msg) |
Return HTTP response with status code. More... | |
void | gos_hs_register_dynamic_page (const gos_hs_dynamic_page_t *page) |
Register dynamic URL callback. More... | |
void | gos_hs_register_header_callback (const gos_hs_custom_header_callback_t callback) |
Register custom header callback. More... | |
void | gos_hs_register_authorize_callback (const gos_hs_authorize_callback_t callback) |
Register unauthorized callback. More... | |
void | gos_hs_register_not_found_callback (const gos_hs_not_found_callback_t callback) |
Register page not found callback. More... | |
gos_hs_param_t * | gos_hs_request_get_param (const gos_hs_request_t *request, const char *key) |
Return GET parameter with specified key. More... | |
gos_hs_header_t * | gos_hs_request_get_header (const gos_hs_request_t *request, const char *key) |
Return request header with specified key. More... | |
gos_hs_method_t | gos_hs_request_get_method (const gos_hs_request_t *request) |
Return the method type of the HTTP request. More... | |
int32_t | gos_hs_request_get_content_length (const gos_hs_request_t *request) |
Return the number of bytes available from the HTTP request. More... | |
gos_result_t | gos_hs_get_tls_client_list (gos_hs_tls_client_t **client_list_ptr) |
Return list of recently connected TLS clients. More... | |
void | gos_hs_destroy_tls_client_list (gos_hs_tls_client_t *client_list) |
Release memory allocated by gos_hs_get_tls_client_list() More... | |
Detailed Description
HTTP server functions.
Function Documentation
◆ gos_hs_authorize_user()
bool gos_hs_authorize_user | ( | const gos_hs_request_t * | request, |
char * | processing_buffer, |
||
const char * | user, |
||
const char * | password |
||
) |
Authorize HTTP request user credentials.
This validates the provided Basic credentials in an HTTP request. More info here
This should be call immediately after a gos_hs_request_processor_t callback. Typically gos_hs_write_unauthorized_response() would be called if this function returns false.
- Parameters
-
request
Internal HTTP request pointer, provided by gos_hs_request_processor_t callback processing_buffer
This is used for internal prcoessing, it should be at least 64 bytes user
The user name to validate against, set to NULL to use the http.server.username setting password
The password to validate against, set to NULL to use the http.server.password setting
- Returns
- gos_result_t result of api call
◆ gos_hs_destroy_tls_client_list()
void gos_hs_destroy_tls_client_list | ( | gos_hs_tls_client_t * | client_list | ) |
Release memory allocated by gos_hs_get_tls_client_list()
- Parameters
-
client_list
List returned by gos_hs_get_tls_client_list()
◆ gos_hs_get_tls_client_list()
gos_result_t gos_hs_get_tls_client_list | ( | gos_hs_tls_client_t ** | client_list_ptr | ) |
Return list of recently connected TLS clients.
Return list of recently connected clients. Up to 8 clients are logged. When the log contains 8 clients and a new client is added, the oldest client is removed. Requires http.server.tls_log_clients to be enabled.
gos_hs_destroy_tls_client_list() must be called to free the memory allocated by the returned list.
See Gecko OS Command API documentation: http.server.tls_client_log.
- Parameters
-
[out] client_list_ptr
Pointer to hold linked list of gos_hs_tls_client_t
◆ gos_hs_is_running()
bool gos_hs_is_running | ( | void |
| ) |
Returns if the HTTP server is running.
- Returns
- true if the HTTP server is running, false else
◆ gos_hs_read_post_data()
gos_result_t gos_hs_read_post_data | ( | const gos_hs_request_t * | request, |
gos_buffer_t * | buffer, |
||
uint32_t | timeout_ms |
||
) |
Read body of HTTP POST request.
This should be used in a gos_hs_request_processor_t callback.
- Parameters
-
request
Internal HTTP request pointer, provided by gos_hs_request_processor_t callback buffer
Pointer to the gos_buffer_t to be filled with the HTTP post body and number of bytes read timeout_ms
Stream read timeout in milliseconds
- Returns
- gos_result_t result of api call
- Examples:
- network/http_server/requests/json_parser.c.
◆ gos_hs_register_authorize_callback()
void gos_hs_register_authorize_callback | ( | const gos_hs_authorize_callback_t | callback | ) |
Register unauthorized callback.
Register callback to be called to authorized username/password of HTTP request. The callback executes in the HTTP server thread.
- Parameters
-
callback
Callback to be called before processing HTTP request, see gos_hs_authorize_callback_t
- Returns
- gos_result_t result of api call
◆ gos_hs_register_dynamic_page()
void gos_hs_register_dynamic_page | ( | const gos_hs_dynamic_page_t * | page | ) |
Register dynamic URL callback.
The callback will be called when the specified URL is requested. The callback executes in the HTTP server thread context.
- Parameters
-
page
URL/callback to register, see gos_hs_dynamic_page_t
- Returns
- gos_result_t result of api call
◆ gos_hs_register_header_callback()
void gos_hs_register_header_callback | ( | const gos_hs_custom_header_callback_t | callback | ) |
Register custom header callback.
Register callback to be called for each HTTP request header. This allows for storing custom HTTP headers in the HTTP request object.
The custom headers are retrieved from the gos_hs_request_t with gos_hs_request_get_header() The callback executes in the HTTP server thread BEFORE the gos_hs_request_processor_t is called.
- Parameters
-
callback
Callback to be called for each HTTP header, see gos_hs_custom_header_callback_t
- Returns
- gos_result_t result of api call
◆ gos_hs_register_not_found_callback()
void gos_hs_register_not_found_callback | ( | const gos_hs_not_found_callback_t | callback | ) |
Register page not found callback.
Register callback to be called if requested URL is not found. The callback executes in the HTTP server thread.
- Parameters
-
callback
Callback to be called if request URL is not found, see gos_hs_not_found_callback_t
- Returns
- gos_result_t result of api call
◆ gos_hs_request_get_content_length()
int32_t gos_hs_request_get_content_length | ( | const gos_hs_request_t * | request | ) |
Return the number of bytes available from the HTTP request.
If the request is chunked encoded then this returns the number of remaining bytes in the current chunk, otherwise this returns the number of bytes in the request body.
- Note
- This should be used in a gos_hs_request_processor_t callback.
- Parameters
-
request
Internal HTTP request pointer, provided by gos_hs_request_processor_t callback
- Returns
- Number of bytes available to be read
◆ gos_hs_request_get_header()
gos_hs_header_t* gos_hs_request_get_header | ( | const gos_hs_request_t * | request, |
const char * | key |
||
) |
Return request header with specified key.
This allows for returning a HTTP header with the given key. Note that only gos_hs_request_header_t are returned with a HTTP request by default. To return custom headers, use gos_hs_register_header_callback() This should be used in a gos_hs_request_processor_t callback.
- Parameters
-
request
Internal HTTP request pointer, provided by gos_hs_request_processor_t callback key
The HTTP header's key value
- Returns
- gos_hs_header_t if header with key found, NULL else
◆ gos_hs_request_get_method()
gos_hs_method_t gos_hs_request_get_method | ( | const gos_hs_request_t * | request | ) |
Return the method type of the HTTP request.
This should be used in a gos_hs_request_processor_t callback.
- Parameters
-
request
Internal HTTP request pointer, provided by gos_hs_request_processor_t callback
- Returns
- The gos_hs_method_t of the current HTTP request
- Examples:
- network/http_server/requests/json_parser.c.
◆ gos_hs_request_get_param()
gos_hs_param_t* gos_hs_request_get_param | ( | const gos_hs_request_t * | request, |
const char * | key |
||
) |
Return GET parameter with specified key.
Returns a GET parameter's value.
A GET request contains parameters of the form:
The get the request's param1, the following code would be used:
This should be used in a gos_hs_request_processor_t callback.
- Parameters
-
request
Internal HTTP request pointer, provided by gos_hs_request_processor_t callback key
The parameter's key value
- Returns
- gos_hs_param_t if key found, NULL else
- Examples:
- network/http_server/requests/get_params.c.
◆ gos_hs_return_status_code()
gos_result_t gos_hs_return_status_code | ( | const gos_hs_request_t * | request, |
uint32_t | code, |
||
const char * | msg |
||
) |
Return HTTP response with status code.
Return a HTTP status code with optional message. The message is printed in the body of the response.
More info about HTTP status codes: here
This should be used in a gos_hs_request_processor_t callback.
- Note
- The HTTP client request is closed after the response is sent.
- Parameters
-
request
Internal HTTP request pointer, provided by gos_hs_request_processor_t callback code
The http status code. msg
Optional message to print in body of response
- Returns
- gos_result_t result of api call
◆ gos_hs_url_decode()
char* gos_hs_url_decode | ( | char * | buffer | ) |
Decode URL encoded string destructively (i.e. in-place)
- Parameters
-
buffer
Pointer to url encoded string
- Returns
- Same pointer as buffer, with contents url decoded
◆ gos_hs_write_chunked_data()
gos_result_t gos_hs_write_chunked_data | ( | const gos_hs_request_t * | request, |
const void * | data, |
||
uint32_t | data_len, |
||
bool | flush_now |
||
) |
Write HTTP body with chunked encoding.
Write the body of a HTTP request using 'Transfer-Encoding: chunked'.
gos_hs_write_reply_header() must be called first with its 'length' parameter set to -1.
This should be used in a gos_hs_request_processor_t callback.
- Parameters
-
request
Internal HTTP request pointer, provided by gos_hs_request_processor_t callback data
Data to write to response data_len
Amount of data to write flush_now
Set to false if there is more data to write, true if this is the last write (which will complete the response)
- Returns
- gos_result_t result of api call
◆ gos_hs_write_data()
gos_result_t gos_hs_write_data | ( | const gos_hs_request_t * | request, |
const void * | data, |
||
uint32_t | data_len, |
||
bool | flush_now |
||
) |
Write HTTP body with non-chunked encoding.
Write the body of the HTTP request using 'Content-Legnth: xxx'
gos_hs_write_reply_header() must be called first with its 'length' parameter > 0.
This should be used in a gos_hs_request_processor_t callback.
- Parameters
-
request
Internal HTTP request pointer, provided by gos_hs_request_processor_t callback data
Data to write to response data_len
Amount of data to write flush_now
Set to false if there is more data to write, true if this is the last write (which will complete the response)
- Returns
- gos_result_t result of api call
◆ gos_hs_write_not_found_response()
gos_result_t gos_hs_write_not_found_response | ( | const gos_hs_request_t * | request | ) |
Return Not Found HTTP response.
Return a 404 Not Found HTTP response
This should be used in a gos_hs_request_processor_t callback.
- Parameters
-
request
Internal HTTP request pointer, provided by gos_hs_request_processor_t callback
- Returns
- gos_result_t result of api call
◆ gos_hs_write_reply_header()
gos_result_t gos_hs_write_reply_header | ( | const gos_hs_request_t * | request, |
const char * | mime_type, |
||
int32_t | length, |
||
gos_hs_response_flag_t | flags |
||
) |
Return HTTP response with a 200 status code.
Completes a HTTP request with a 200 status code.
This should be used in a gos_hs_request_processor_t callback.
- Note
- To return a non-200 code, see gos_hs_return_status_code()
- Parameters
-
request
Internal HTTP request pointer, provided by gos_hs_request_processor_t callback mime_type
The response 'Content-Type', set NULL if unused length
The 'Content-Length' if > 0, set to -1 for 'Transfer-Encoding: chunked' flags
Optionals flags to add to the response headers, gos_hs_response_flag_t
- Returns
- gos_result_t result of api call
◆ gos_hs_write_reply_header_with_config()
gos_result_t gos_hs_write_reply_header_with_config | ( | const gos_hs_request_t * | request, |
const gos_hs_reply_config_t * | config |
||
) |
Return HTTP response with specified configuration.
Completes a HTTP request with the specified configuration
This should be used in a gos_hs_request_processor_t callback.
- Parameters
-
request
Internal HTTP request pointer, provided by gos_hs_request_processor_t callback config
The reply configuration, see gos_hs_reply_config_t
- Returns
- gos_result_t result of api call
◆ gos_hs_write_unauthorized_response()
gos_result_t gos_hs_write_unauthorized_response | ( | const gos_hs_request_t * | request | ) |
Return Unauthorized HTTP response.
Return a 403 Unauthorized HTTP response
This should be used in a gos_hs_request_processor_t callback.
- Parameters
-
request
Internal HTTP request pointer, provided by gos_hs_request_processor_t callback
- Returns
- gos_result_t result of api call