Gecko OS is part of a larger sophisticated application framework installed on all Gecko OS devices. ... reboot ... wlan.network.gateway wlan.network.ip wlan.network.netmask wlan.network.status
ProductWirelessResource TypeSoftware API documentation
Gecko OS 4.2 Command API The Command API documentation provides details of commands and variables as well as lots of Command API examples covering a wide range of uses.
... PSA Crypto is the recommended device independent crypto API and should be used whenever possible. ... the device will erase OTP and become inoperable if 4 glitch signals is seen in a 1 minute ...
// Gecko Platform//Version 4.4.1 //Services ... All API functions can be called from within interrupt handlers. ... sl_sleeptimer_is_power_manager_early_restore_timer_latest_to_expire(void)
Results 1-5 of 5 for gecko-os/4/standard/latest/sdk/api/gos_network_ping