WGM160P Gecko OS Plugin peripheral.dac ... update - optional: invoke a DFU after successful activation ... Gecko OS writes the file to extended flash or bulk flash, depending on the location ...
Gecko OS 4.2 Command API The Command API documentation provides details of commands and variables as well as lots of Command API examples covering a wide range of uses.
... page provides a list of Bluetooth Xpress API commands with a full description of how ... os pins can only use the strong drive strength. ... Output, open-source with pull-up (see gdi os pren )
ProductWirelessResource TypeSoftware API documentation
// Gecko Platform//Version 4.4.1 //Services ... All API functions can be called from within interrupt handlers. ... sl_sleeptimer_is_power_manager_early_restore_timer_latest_to_expire(void)
Results 1-5 of 5 for gecko-os/4/standard/latest/sdk/api/gos_ntp_update