Gecko OS is part of a larger sophisticated application framework installed on all Gecko OS devices. ... reboot ... wlan.scan.num_probes wlan.scan.passive_dwell wlan.scan.retries wlan.scan.type
ProductWirelessResource TypeSoftware API documentation
Gecko OS 4.2 Command API The Command API documentation provides details of commands and variables as well as ... Overview for a description of the general structure and features of Gecko OS 4.
Issue Gecko OS command, store string result in buffer. ... Issue Gecko OS command, return result data in buffer. ... Examples: network/ethernet_bridge/main.c . ◆ gos_cmd_issue_with_data()
ProductWirelessResource TypeSoftware API documentation
os pins can only use the strong drive strength. ... scan accepts an optional <threshold> argument. ... scan off scan results scan high -20dBm Example scan high ! # RSSI BD_ADDR Device Name
ProductWirelessResource TypeSoftware API documentation
This document describes using the Flex SDK for 802.15.4 development on EFR32™ Wireless parts. ... 4.3.1 Enable Address Filtering HW accelerated MAC features, such as frame and address ...
Resource TypeApplication Notes
Results 1-5 of 5 for gecko-os/4/standard/latest/sdk/api/gos_spi_stream_configure