Gecko OS is part of a larger sophisticated application framework installed on all Gecko OS devices. ... See Device Firmware Update . The Device Management Server (DMS) To update a Gecko OS ...
ProductWirelessResource TypeSoftware API documentation
Gecko OS 4.2 Command API The Command API documentation provides details of commands and variables as well as lots of Command API examples covering a wide range of uses.
... that PSA Crypto is the recommended device independent crypto API and should be used whenever possible. ... Reset period Trigger threshold These options can be set to the values given in the ...
// Gecko Platform//Version 4.4.1 //Services ... All API functions can be called from within interrupt handlers. ... sl_sleeptimer_is_power_manager_early_restore_timer_latest_to_expire(void)
Results 1-5 of 5 for gecko-os/4/standard/latest/sdk/api/gos_tcp_trigger_server_event_handlers