Custom Commands Example

Demonstrates how to register custom serial commands with Gecko OS. Also demonstrates have to save and load settings from NVM.

API Features Demonstrated

Platforms

This app works on:

Requirements and Prerequisites

Requires a Gecko OS evaluation board, such as a WGM160P_eval.

Description

Registers commands to start and stop polling of humidity and temperature sensor values.

Registers custom variables to enable or disable humidity and temperature sensor polling and to set polling periods.

Registers additional variables to get and set cloud values.

Provides help for the new commands and variables.

Source Code

See: