Basic Device Setup Example

Demonstrates how to use the Web Setup webapp in both setup and normal modes.

API Features Demonstrated

Platforms

This app works on:

Requirements and Prerequisites

Requires a Gecko OS evaluation board, such as a WGM160P_eval.

Description

Loads settings.

Registers an event handler for the network event.

Registers an setup finished handler.

Calls start_network_interface()

The start_network_interface() function tries to start the WLAN interface. If it fails it starts web setup.

Source Code

See: