Basic UDP Hello GPIO Example

UDP Client sends GPIO values to a remote server

API Features Demonstrated

Platforms

This app works on:

Requirements and Prerequisites

Requires a Gecko OS evaluation board, such as a WGM160P_eval.

Other Gecko OS hardware can also be used by changing the source of the logged data to suit your device.

Description

This is a basic UDP client application. The app:

Usage Instructions

Open a Gecko OS serial terminal to the device. See Getting Started, Opening a Gecko OS Terminal.

This app assumes your Gecko OS device is set up with the credentials to join your local network. If you have not already set up network credentials, on the Gecko OS terminal, run the commands:

network_up -s
save

See the Wi-Fi Command API documentation for network_up and save.

After building, downloading and running the app, it joins the network and connects to the test server.

Output on the Gecko OS terminal is as follows:

> Connecting to remote UDP server test.zentri.com:50007
Sending data
Finished

Source

See: