Silicon Labs
gecko-os/4/standard/latest/sdk/hurricane-security-camera-resources-cloud-server-public-src-boot-firebase-firestore-js-example
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
      Results 1-5 of 5 for gecko-os/4/standard/latest/sdk/hurricane-security-camera-resources-cloud-server-public-src-boot-firebase-firestore-js-example in 0.04 seconds
      Understanding the Bluetooth Connection Process | Connections | Bluetooth LE | v5.0 | Silicon Labs
      https://docs.silabs.com/.../understanding-the-bluetooth-connection-proc...
      Bluetooth ensures reliable data transfers for connected devices. ... The advertising data can be seen by any device within range but it is not possible to establish a connection.
      Optimizing Current Consumption in Bluetooth Low Energy Devices | System & Performance | Bluetooth LE | v5.0 | Silicon Labs
      https://docs.silabs.com/.../optimizing-current-consumption-in-bluetooth-low-energy-devi...
      0 dBm is enough to cover about 10 to 15 m range, based on tests made with iBeacon ... The same TX power level setting (sl_bt_system_set_tx_power()) applies to advertisements and connections.
      Adaptive Frequency Hopping | System & Performance | Bluetooth LE | v5.0 | Silicon Labs
      https://docs.silabs.com/.../adaptive-frequency-hopp...
      // Bluetooth LE//Version 5.0 //General //System & Performance ... Bluetooth Low Energy has two channel selection algorithms. ... The selected channel appears to be semi-random.
      Setting a Custom BT Address - Production Approach | System & Performance | Bluetooth LE | v5.0 | Silicon Labs
      https://docs.silabs.com/.../setting-a-custom-bt-address-production-appro...
      // Bluetooth LE//Version 5.0 //General //System & Performance ... , subtract six flash pages from the end address of the main flash (5 pages for the NVM3 and 1 page for manufacturing tokens).
      Creating an Eddystone-URL Beacon | Advertising & Scanning | Bluetooth LE | v2.13 | Silicon Labs
      https://docs.silabs.com/....
      // Bluetooth LE//Version 2.13 // ... demonstrates how to create an Eddystone beacon with Silicon Labs' Bluetooth SDK. ... The Eddystone-URL packet advertises a URL in a compressed format.
        Results 1-5 of 5 for gecko-os/4/standard/latest/sdk/hurricane-security-camera-resources-cloud-server-public-src-boot-firebase-firestore-js-example