Gecko OS is part of a larger sophisticated application framework installed on all Gecko OS devices. ... factory_reset command with the returned MAC address as its argument:
ProductWirelessResource TypeSoftware API documentation
Gecko OS 4.2 Command API The Command API documentation provides details of commands and variables as well as ... Overview for a description of the general structure and features of Gecko OS 4.
Issue Gecko OS command, store string result in buffer. ... Issue Gecko OS command, return result data in buffer. ... Examples: network/ethernet_bridge/main.c . ◆ gos_cmd_issue_with_data()
ProductWirelessResource TypeSoftware API documentation
Example Example usage. Alphabetical List of Commands ... Factory reset deletes the entire user dynamic area, including user saved ... os pins can only use the strong drive strength.
ProductWirelessResource TypeSoftware API documentation
This document describes using the Flex SDK for 802.15.4 development on EFR32™ Wireless parts. ... 4.1 Applying a PHY from RAIL rx 0 // Configs can be loaded only in radio Idle state ...
Resource TypeApplication Notes
Results 1-5 of 5 for gecko-os/4/standard/latest/sdk/manufacturing-factory-image-main-c-example