Configuration Options The API Flow Control Support ... the UARTDRV_InitLeuart() function for LEUART peripherals. The API This section contains brief descriptions of the functions in the API.
ProductMicrocontrollersResource TypeSoftware API documentation
You are viewing documentation for version: 4.2 | Version History ... The control block references a ring buffer for each configured channel. ... You should avoid using it in production.
ProductMicrocontrollersResource TypeSoftware API documentation
// Gecko Platform//Version 4.4.1 //Services ... All API functions can be called from within interrupt handlers. ... sl_sleeptimer_is_power_manager_early_restore_timer_latest_to_expire(void)
Login ... // Platform//Version 5.0.1 //Security //API Documentation //SE Manager ... Note that PSA Crypto is the recommended device independent crypto API and should be used whenever possible.
Results 1-5 of 5 for gecko-os/4/standard/latest/sdk/network-http-methods-common-h-example