Gecko OS 4.2 Command API The Command API documentation provides details of commands and variables as well as ... Overview for a description of the general structure and features of Gecko OS 4.
Issue Gecko OS command, store string result in buffer. ... Issue Gecko OS command, return result data in buffer. ... Examples: network/ethernet_bridge/main.c . ◆ gos_cmd_issue_with_data()
ProductWirelessResource TypeSoftware API documentation
Gecko OS is part of a larger sophisticated application framework installed on all Gecko OS devices. ... format_flash get ls ... get wlan.mac to obtain the device MAC address
ProductWirelessResource TypeSoftware API documentation
os pins can only use the strong drive strength. ... Get the current value of a general purpose I/O pin configured for the stdio function. ... Get a list of values for all GPIOs at once.
ProductWirelessResource TypeSoftware API documentation
... application (e.g., putting them below FreeRTOS OS atomic for access to OS functions in RAIL callbacks). ... viewing transmitted and received radio packets for network sniffing or debugging.
Resource TypeSoftware API Documentation
Results 1-5 of 5 for gecko-os/4/standard/latest/sdk/network-http-methods-http-get-c-example