http_head http_post http_read_status ... Gecko OS writes the file to extended flash or bulk flash, depending on the location option ... c rc: CRC32 checksum of the file data, in hex format 2 .
Issue Gecko OS command, store string result in buffer. ... Issue Gecko OS command, return result data in buffer. ... Examples: network/ethernet_bridge/main.c . ◆ gos_cmd_issue_with_data()
ProductWirelessResource TypeSoftware API documentation
Gecko OS 4.2 Command API The Command API documentation provides details of commands and variables as well as ... Overview for a description of the general structure and features of Gecko OS 4.
C:\SiliconLabs\SimplicityStudio\v5\developer\adapter_packs\commander ... For Linux OS, the path in step 4 is also different. ... Set the preferred SDK to Gecko SDK Suite v 3.1.1 or newer.