Silicon Labs
gecko-os/4/standard/latest/sdk/system-custom-commands-main-c-example
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
    Results 1-5 of 5 for gecko-os/4/standard/latest/sdk/system-custom-commands-main-c-example in 0.23 seconds
    Gecko OS 4.2 Command API Silicon Labs
    https://docs.silabs.com/.../...
    Gecko OS 4.2 Command API The Command API documentation provides details of commands and variables as well as ... Overview for a description of the general structure and features of Gecko OS 4.
    Commands - v4.1 - Gecko OS API Documentation Silicon Labs
    https://docs.silabs.com/.../group-api-core-comm...
    Issue Gecko OS command, store string result in buffer. ... Issue Gecko OS command, return result data in buffer. ... Examples: network/ethernet_bridge/main.c . ◆ gos_cmd_issue_with_data()
    ProductWireless Resource TypeSoftware API documentation
    Update and Recovery - v4.1 - Gecko OS API Documentation Silicon Labs
    https://docs.silabs.com/.../update-and-recov...
    Gecko OS is part of a larger sophisticated application framework installed on all Gecko OS devices. ... The Gecko OS Device Firmware Update (DFU) feature allows device firmware to be updated ...
    ProductWireless Resource TypeSoftware API documentation
    EFR32 | Silicon Labs RAIL API Reference Guide | RAIL | v2.15 | Silicon Labs
    https://docs.silabs.com/.../efr32-m...
    ... while EFR32xG22 and later platforms require 4-byte alignment; applications can use ... application (e.g., putting them below FreeRTOS OS atomic for access to OS functions in RAIL callbacks).
    Resource TypeSoftware API Documentation
    BGX13-1.x Command Reference - v1.0 - Gecko OS API Documentation Silicon Labs
    https://docs.silabs.com/.../comma...
    Example Example usage. Alphabetical List of Commands ... os pins can only use the strong drive strength. ... Returns the RSSI value from the latest received packet of the current active ...
    ProductWireless Resource TypeSoftware API documentation
      Results 1-5 of 5 for gecko-os/4/standard/latest/sdk/system-custom-commands-main-c-example