Silicon Labs
gecko-os/4/standard/latest/sdk/system-system-monitor-system-monitor-mk-example
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
Results 1-5 of 5 for gecko-os/4/standard/latest/sdk/system-system-monitor-system-monitor-mk-example in 0.18 seconds
UARTDRV - UART Driver - v4.2 - Gecko Platform API Documentation Silicon Labs
https://docs.silabs.com/.../group-uart...
Example ... Also define the CTS and RTS locations by setting portLocationCts and portLocationRts in the init struct. ... [in] type Abort type – whether to abort only Tx, only Rx, or both.
ProductMicrocontrollers Resource TypeSoftware API documentation
Sleep Timer | API Documentation | Gecko Platform | v4.4.1 | Silicon Labs
https://docs.silabs.com/.../sleepti...
// Gecko Platform//Version 4.4.1 //Services ... All API functions can be called from within interrupt handlers. ... sl_sleeptimer_is_power_manager_early_restore_timer_latest_to_expire(void)
Project Configurator and Gecko Platform
https://www.silabs.com/.../project-configuration-gecko-platform-training....
... -platform/latest/driver/api/group-uartdrv https://docs.silabs.com/gecko-platform/latest/driver/api/group-ustimer Gecko Platform – Service ... Platform Services Detail Device Initialization
I/O Stream RTT - v4.2 - Gecko Platform API Documentation Silicon Labs
https://docs.silabs.com/.../group-iostream-...
sl_status_t sl_iostream_rtt_init (void) RTT Stream init. Variables ... Function Documentation ◆ sl_iostream_rtt_init() sl_status_t sl_iostream_rtt_init ... ) RTT Stream init. Returns
ProductMicrocontrollers Resource TypeSoftware API documentation
SE Manager | API Documentation | Platform | v5.0.1 | Silicon Labs
https://docs.silabs.com/.../sl-se-mana...
// Platform//Version 5.0.1 //Security ... is the recommended device independent crypto API and should be used whenever possible ... sl_se_otp_init_t otp_settings_init = SL_SE_OTP_INIT_DEFAULT;
    Results 1-5 of 5 for gecko-os/4/standard/latest/sdk/system-system-monitor-system-monitor-mk-example