Gecko OS 4.2 Command API The Command API documentation provides details of commands and variables as well as ... Overview for a description of the general structure and features of Gecko OS 4.
Issue Gecko OS command, store string result in buffer. ... Issue Gecko OS command, return result data in buffer. ... Examples: network/ethernet_bridge/main.c . ◆ gos_cmd_issue_with_data()
ProductWirelessResource TypeSoftware API documentation
Gecko OS is part of a larger sophisticated application framework installed on all Gecko OS devices. ... to update the firmware, or switch back to Gecko OS using the faults_reset command.
ProductWirelessResource TypeSoftware API documentation
SPI spi_master_config spi_master_open ... Gecko OS writes the file to extended flash or bulk flash, depending on the location ... c rc: CRC32 checksum of the file data, in hex format 2 .
Example Example usage. Alphabetical List of Commands ... If more time is needed to set up test equipment between the end of advertising and ... os pins can only use the strong drive strength.
ProductWirelessResource TypeSoftware API documentation
Results 1-5 of 5 for gecko-os/4/standard/latest/sdk/test-spi-loop-back-main-c-example