Gecko OS is part of a larger sophisticated application framework installed on all Gecko OS devices. ... The Gecko OS Device Firmware Update (DFU) feature allows device firmware to be updated ...
ProductWirelessResource TypeSoftware API documentation
Gecko OS 4.2 Command API The Command API documentation provides details of commands and variables as well as ... Overview for a description of the general structure and features of Gecko OS 4.
Modules ... [out] buffer Buffer to hold returned data [in] ... [out] buffer Buffer to hold string result [in] ... Issue Gecko OS command asynchronously and invoke callback on completion.
ProductWirelessResource TypeSoftware API documentation
Example Example usage. Alphabetical List of Commands ... os pins can only use the strong drive strength. ... Returns the RSSI value from the latest received packet of the current active ...
ProductWirelessResource TypeSoftware API documentation
This document describes using the Flex SDK for 802.15.4 development on EFR32™ Wireless parts. ... 4.1 Applying a PHY from RAIL rx 0 // Configs can be loaded only in radio Idle state ...
Resource TypeApplication Notes
Results 1-5 of 5 for gecko-os/4/standard/latest/sdk/utility-buffer-dump-main-c-example