Gecko OS 4.2 Command API The Command API documentation provides details of commands and variables as well as ... Overview for a description of the general structure and features of Gecko OS 4.
Gecko OS is part of a larger sophisticated application framework installed on all Gecko OS devices. ... Safe mode operation is guaranteed in the unlikely event the device is configured in a ...
ProductWirelessResource TypeSoftware API documentation
Modules ... Issue Gecko OS command, store string result in buffer. ... More. gos_result_t gos_cmd_issue_with_vconfig ( gos_cmd_operation_config_t *config, const char *fmt, va_list args)
ProductWirelessResource TypeSoftware API documentation
os pins can only use the strong drive strength. ... Output, push-pull 4 Output, open-drain with no pull-up (see gdi od prdi ) ... A list of available functions is shown in the following table.
ProductWirelessResource TypeSoftware API documentation
... the standard PHYs defined by the 802.15.4 PHY layer specification, it is possible to ... 4.3.1 Enable Address Filtering HW accelerated MAC features, such as frame and address filtering, are ...
Resource TypeApplication Notes
Results 1-5 of 5 for gecko-os/4/standard/latest/structgos-safe-slinked-list-t