Silicon Labs
gecko-os/4/standard/latest/structgos-scan-result-t
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
    Results 1-5 of 5 for gecko-os/4/standard/latest/structgos-scan-result-t in 0.21 seconds
    Gecko OS 4.2 Command API Silicon Labs
    https://docs.silabs.com/.../...
    Gecko OS 4.2 Command API The Command API documentation provides details of commands and variables as well as ... Overview for a description of the general structure and features of Gecko OS 4.
    Update and Recovery - v4.1 - Gecko OS API Documentation Silicon Labs
    https://docs.silabs.com/.../update-and-recov...
    Gecko OS is part of a larger sophisticated application framework installed on all Gecko OS devices. ... reboot ... wlan.scan.num_probes wlan.scan.passive_dwell wlan.scan.retries wlan.scan.type
    ProductWireless Resource TypeSoftware API documentation
    Commands - v4.1 - Gecko OS API Documentation Silicon Labs
    https://docs.silabs.com/.../group-api-core-comm...
    Command data types. ... Issue Gecko OS command, return result data in buffer. ... fmt Formatted Gecko OS command Returns gos_result_t result of api call ◆ gos_cmd_issue_with_callback()
    ProductWireless Resource TypeSoftware API documentation
    BGX13-1.x Command Reference - v1.0 - Gecko OS API Documentation Silicon Labs
    https://docs.silabs.com/.../comma...
    os pins can only use the strong drive strength. ... Scan intervals and configuration are defined by ce s h d , ce s h i , ce s l d , and ce s ... scan accepts an optional <threshold> argument.
    ProductWireless Resource TypeSoftware API documentation
    Gecko OS Commands Silicon Labs
    https://docs.silabs.com/.../comma...
    wlan_get_rssi wlan_scan GPIOs and Peripherals ... Gecko OS writes the file to extended flash or bulk flash, depending on the location ... t ype: specify file type as integer or hex string 2 .
      Results 1-5 of 5 for gecko-os/4/standard/latest/structgos-scan-result-t