Gecko OS is part of a larger sophisticated application framework installed on all Gecko OS devices. ... network.tls.ca_cert spi.master.active_gpio spi.master.active_level system.cmd.buffered
ProductWirelessResource TypeSoftware API documentation
Gecko OS 4.2 Command API The Command API documentation provides details of commands and variables as well as lots of Command API examples covering a wide range of uses.
Modules Types Command data types. Functions ... Issue Gecko OS command, store string result in buffer. ... ) Issue Gecko OS Command. For available commands, see Gecko OS Command API . ... Note
ProductWirelessResource TypeSoftware API documentation
Gecko OS evaluation boards are by default configured to enter Setup Web mode when you hold down Button 2 ... As well as standard Gecko OS terminal behavior, the Console tab provides additional ...
... page provides a list of Bluetooth Xpress API commands with a full description of how ... os pins can only use the strong drive strength. May be one of the following types: drvst : Strong drive ...
ProductWirelessResource TypeSoftware API documentation
Results 1-5 of 5 for gecko-os/4/standard/latest/structgos-spi-device-t