Gecko OS is part of a larger sophisticated application framework installed on all Gecko OS devices. ... system.safemode.sleep_timeout - Set the duration for which the device sleeps before ...
ProductWirelessResource TypeSoftware API documentation
Issue Gecko OS command, return the uint32 result. ... Issue Gecko OS command, store string result in buffer. ... ) Issue Gecko OS Command. For available commands, see Gecko OS Command API .
ProductWirelessResource TypeSoftware API documentation
Gecko OS 4.2 Command API The Command API documentation provides details of commands and variables as well as lots of Command API examples covering a wide range of uses.
Gecko OS evaluation boards are by default configured to enter Setup Web mode when you hold down Button 2, press Reset, and ... The Gecko OS file system does not support directories or folders.
... in the examples on this page were captured with system print level ( sy p ) = all, and system command header enabled ( sy c h ) = true. ... os pins can only use the strong drive strength.
ProductWirelessResource TypeSoftware API documentation
Results 1-5 of 5 for gecko-os/4/standard/latest/structgos-ssid-t