Silicon Labs
gecko-os/4/standard/latest/structgos-version-details-t
Clear
SearchLoading
Explore a fresh approach to searching with our
AI-driven document search.
powered by
  • Docs Home
  • DocSpace
  • Last Page Titlle
  • Docs Search
Relevancy Latest
Filter by:
Filter by:
Filter by:
Narrow By
Collapse All

Software Docs

Loading

Products

Loading

Resource Type

Loading

Language

Loading
Clear All Filters

All Results

Software Docs

Products

Results 1-5 of 5 for gecko-os/4/standard/latest/structgos-version-details-t in 0.17 seconds
Gecko OS 4.2 Command API Silicon Labs
https://docs.silabs.com/.../...
Gecko OS 4.2 Command API The Command API documentation provides details of commands ... See Gecko OS General Overview for a description of the general structure and features of Gecko OS 4.
Update and Recovery - v4.1 - Gecko OS API Documentation Silicon Labs
https://docs.silabs.com/.../update-and-recov...
Update and Recovery Gecko OS is part of a larger sophisticated application framework installed on all Gecko OS devices. ... reboot ... system.uuid system.version tcp.client.connect_timeout
ProductWireless Resource TypeSoftware API documentation
Commands - v4.1 - Gecko OS API Documentation Silicon Labs
https://docs.silabs.com/.../group-api-core-comm...
Issue Gecko OS command, store string result in buffer. ... Issue Gecko OS command, return result data in buffer. ... Command configuration, see gos_cmd_operation_config_t for more details.
ProductWireless Resource TypeSoftware API documentation
BGX13-1.x Command Reference - v1.0 - Gecko OS API Documentation Silicon Labs
https://docs.silabs.com/.../comma...
os pins can only use the strong drive strength. ... for nearby Bluetooth Xpress peripherals Version Notes Starting with version 1.1.1229.0 , the BLE PHY used for scanning is determined by bl ...
ProductWireless Resource TypeSoftware API documentation
AN1365: 15.4 over RAIL
https://www.silabs.com/.../an1365-15-4-over-rail....
... the standard PHYs defined by the 802.15.4 PHY layer specification, it is possible to ... 4.7.2 Dynamic FEC SUN FSK protocol defines the dynamic FEC feature which is supported on certain EFR32 ...
Resource TypeApplication Notes
    Results 1-5 of 5 for gecko-os/4/standard/latest/structgos-version-details-t