Gecko OS 4.2 Command API The Command API documentation provides details of commands and variables as well as ... Overview for a description of the general structure and features of Gecko OS 4.
Gecko OS writes the file to extended flash or bulk flash, depending on the location option: -l extended/bulk . ... [Disassociated] SILABS-WGM160P-4.0.0, Gecko_OS-STANDARD-4.0.12-1198, WGM160P
Issue Gecko OS command, store string result in buffer. ... Issue Gecko OS command, return result data in buffer. ... Issue Gecko OS command asynchronously and invoke callback on completion.
ProductWirelessResource TypeSoftware API documentation
Update and Recovery Gecko OS is part of a larger sophisticated application framework installed on all Gecko OS devices. ... claim - associate a particular device with your user account.
ProductWirelessResource TypeSoftware API documentation
Factory reset deletes the entire user dynamic area, including user saved configurations. ... os pins can only use the strong drive strength. ... Example Save user configuration. > save
ProductWirelessResource TypeSoftware API documentation
Results 1-5 of 5 for gecko-os/4/standard/latest/user-guide/getting-started