Gecko OS is part of a larger sophisticated application framework installed on all Gecko OS devices. ... format_flash get ls ... get wlan.mac to obtain the device MAC address
ProductWirelessResource TypeSoftware API documentation
Issue Gecko OS command, store string result in buffer. ... Issue Gecko OS command, return result data in buffer. ... Issue Gecko OS command asynchronously and invoke callback on completion.
ProductWirelessResource TypeSoftware API documentation
Gecko OS 4.2 Command API The Command API documentation provides details of commands and variables as well as ... Overview for a description of the general structure and features of Gecko OS 4.
Gecko OS evaluation boards are by default configured to enter Setup Web mode when you ... HTTP and REST API server listening on port: 80 ... You can issue any Gecko OS command from this page.
os pins can only use the strong drive strength. ... Get a list of values for all GPIOs at once. ... Returns the RSSI value from the latest received packet of the current active connection.
ProductWirelessResource TypeSoftware API documentation
Results 1-5 of 5 for gecko-os/4/standard/latest/variables/ethernet