Host Boot

hboot.filename

Abbreviation

hb f

Access

get/set

Description

Set the default value of the host boot filename.

See hboot command.

Arguments

<filename>

where filename is name of the firmware file from which to boot.

Default

host_firmware.bin

Get example

> get hb f
R000019
host_firmware.bin

Set example

> set hb f EFM8/UB1/SpaceInvaders.efm8
R000008
Set OK