Gecko OS Variables
This page provides a list of Gecko OS variables with a full description of the function of each variable together with example usage.
Variables are cached in volatile RAM and must be saved to non-volatile flash memory to persist between reboots. To save variables to flash, use the save command. Some variables impact the operation of the entire system, wake and sleep timers for example. A save and reboot is required before new settings for these types of variables take effect.
Variable settings can be loaded using the load command.
The get and set Command API functions are used to read and write Gecko OS variables respectively.
Shortcuts
A shortcut is assigned to each variable. The format for shortcuts is shown in the following table. The shortcut is a hybrid of the first two characters of the first word of the variable name, plus (typically) the first character of the second word (if a second word exists), plus (typically) the first character of the third word of the variable name (if a third word exists). Each of these characters is separated by a space character. In some instances, it was not possible to use the first letter of the second or third word in the variable name, in these cases another letter has been somewhat arbitrarily chosen.
Variable Name | Shortcut | |
---|---|---|
Template | first_word.second_word.third_word | fi s t |
Example 1 | time.uptime | ti u |
Example 2 | wlan.scan.retries | wl s r |
Documentation Format
Many Gecko OS responses shown in the examples on this page were captured with system.print_level = 0, and system.cmd.header_enabled = 1. These machine friendly settings make it easy for a host MCU to parse responses by examining response headers. Documentation for each variable is provided in the format shown below.
variable
Abbreviation
var
Access
get/set
Description
A description of the function of the variable.
Arguments
A full list of mandatory and optional arguments.
Default
The factory reset default value.
Get example
An example of how to read the variable, including response codes.
Set example
An example of how to write the variable, including response codes (for writeable variables).
NOTE! Don't forget to check out command navigation tips to make it easier to find and type specific variable names.
List of Variables
- All Variables
- Broadcast
- Bus
- DMS
- GPIO
- HTTP Server
- IO Connection
- Network
- NTP
- Remote Terminal
- Setup
- SoftAP Interface
- System
- system.build_number
- system.cmd.echo
- system.cmd.header_enabled
- system.cmd.mode
- system.cmd.prompt_enabled
- system.gotosleep.timeout
- system.indicator.gpio
- system.indicator.state
- system.memory.usage
- system.oob.event_mask
- system.oob.gpio
- system.oob.gpio_level
- system.oob.rising_edge_mask
- system.oob.status
- system.print_level
- system.safemode.disabled
- system.safemode.status
- system.uuid
- system.version
- system.wakeup.timeout
- TCP Client
- TCP Server
- Time
- UART
- UDP Client
- UDP Server
- WLAN Interface
- wlan.auto_join.enabled
- wlan.auto_join.retries
- wlan.auto_join.retry_delay
- wlan.dhcp.enabled
- wlan.dhcp.hostname
- wlan.hide_passkey
- wlan.info
- wlan.join.retries
- wlan.join.timeout
- wlan.mac
- wlan.network.dns
- wlan.network.gateway
- wlan.network.ip
- wlan.network.netmask
- wlan.network.status
- wlan.passkey
- wlan.rate.protocol
- wlan.ssid
- wlan.static.dns
- wlan.static.gateway
- wlan.static.ip
- wlan.static.netmask
- wlan.tx_power
Variable Properties
The table below indicates properties of variables:
- When a change in variable value takes effect:
Immediate
- a change in the variable value takes effect immediatelyuart_update
- run the uart_update command to apply a change in the variable valueNetwork Restart
- restart the network to apply a change in the variable valueSetup Restart
- restart the web setup to apply a change in the variable valueSave/Reboot
- a save and reboot is required to apply a change in the variable value
Safe Mode
- variable is available in safe mode