WLAN Interface
wlan.auto_join.enabled
Abbreviation
wl o e
Access
get/set
Description
Enable/disable network auto-join using the wlan interface on bootup.
Arguments
<0/off/false/1/on/true>
Default
0
Properties
- network_restart to apply change
Get example
> get wl o e
R000003
0
Set example
> set wl o e true
R000008
Set OK
wlan.auto_join.retries
Abbreviation
wl o r
Access
get/set
Description
Maximum number of attempts to auto-join a network. 0 = retry indefinitely.
Arguments
<0-255>
Default
3
Properties
Get example
> get wl o r
R000003
3
Set example
> set wl o r 5
R000008
Set OK
wlan.auto_join.retry_delay
Abbreviation
wl o d
Access
get/set
Description
The period between auto-join attempts in seconds.
Arguments
<0-255>
Default
10
Properties
Get example
> get wl o d
R000004
10
Set example
> set wl o d 5
R000008
Set OK
wlan.dhcp.enabled
Abbreviation
wl d e
Access
get/set
Description
Select whether DHCP is used to automatically obtain an IPv4 IP address on the wlan interface.
Note: Renamed from network.dhcp
after Gecko OS v1.2. Renamed from network.dhcp.enabled
in Gecko OS 3.0.
See Networking and Security, DHCP Client.
Arguments
<0/off/false/1/on/true>
Default
1
Properties
- network_restart to apply change
- available in Safe Mode
- preserved by NVM Backup
Get example
> get wl d e
R000003
1
Set example
> set wl d e off
R000008
Set OK
wlan.dhcp.hostname
Abbreviation
wl d h
Access
get/set
Description
Configures the DHCP client's hostname (DHCP option 12) sent to the DHCP server.
See Networking and Security, DHCP Client.
Arguments
<hostname>
Default
Silabs-#
where #
is replaced by the last three digits of the WLAN MAC address
Properties
- network_restart to apply change
Get example
> get wl d h
R000009
Silabs-#
Set example
> set wl d h my_dhcp_client
R000008
Set OK
wlan.hide_passkey
Abbreviation
wl h
Access
get/set
Description
Hide the variable wlan.passkey. Once hidden, a factory reset must be issued to reset this variable and reveal the (reset value) of the passkey.
Note: Don't forget to save before reboot!
Arguments
<0/off/false/1/on/true>
Default
0
Properties
- available in Safe Mode
- preserved by NVM Backup
Get example
> get wl h
R000003
0
Set example
> set wl h true
R000008
Set OK
> save
R000009
Success
> get wlan.passkey
R000008
******
wlan.info
Abbreviation
wl i
Access
get
Description
WLAN connection status parameters: state, SSID, BSSID, channel and datarate
Arguments
-
Default
<varies>
Get example
> get wlan.info
state: up
SSID: Silabs
BSSID: 30:85:A9:E7:9C:B0
channel: 6
datarate: 450.0
wlan.join.retries
Abbreviation
wl j r
Access
get/set
Description
Specifies the maximum number of attempts to join a WLAN network after issuing the network_up command (or any other command requiring network access when the network is down).
If the network_down command is issued while attempting to join a network, the subsequent attempts are canceled.
Note that wlan.join.retries is separate from the wlan.auto_join.retries variable. If wlan.auto_join.retries > 0, then the total number of retries is calculated by the multiplication of wlan.join.retries with wlan.auto_join.retries.
Arguments
<retries>
where '
Default
3
Properties
- network_restart to apply change
- available in Safe Mode
- preserved by NVM Backup
Get example
> get wl j r
R000003
5
Set example
> set wl j r 5
R000008
Set OK
wlan.join.timeout
Abbreviation
wl j t
Access
get/set
Description
The maximum amount of time to wait while the module attempts to join a network.
Arguments
<timeout in ms>
Default
7000 ms
Properties
- save and reboot to apply change
- available in Safe Mode
- preserved by NVM Backup
Get example
> get wlan.join.timeout
R000006
7000
Set example
> set wl j t 5000
R000008
Set OK
wlan.mac
Abbreviation
wl m
Access
get
Description
Returns the wlan MAC address.
Arguments
-
Default
varies
Properties
- available in Safe Mode
Get example
> get wl m
R000019
4C:55:CC:01:23:45
wlan.network.dns
Abbreviation
wl n d
Access
get
Description
Return a comma separated list of the DNS server addresses that the wlan interface is using.
Note: To set a static DNS address list, use the wlan.static.dns variable.
See Networking and Security, DNS Client
Arguments
-
Default
0.0.0.0
(i.e. No DNS addresses in use)
Properties
- available in Safe Mode
Get example
> get wl n d
10.5.6.1
wlan.network.gateway
Abbreviation
wl n g
Access
get
Description
Returns the wlan interface IPv4 gateway IP address resolved by DHCP.
Note: To set a static gateway, use the wlan.static.gateway variable.
Arguments
-
Default
0.0.0.0
Properties
- available in Safe Mode
Get example
> get wl n g
R000013
192.168.0.1
wlan.network.ip
Abbreviation
wl n i
Access
get
Description
Returns the wlan interface IPv4 IP address resolved by DHCP.
Note: To set a static IP address, use the wlan.static.ip variable.
Arguments
-
Default
0.0.0.0
Properties
- available in Safe Mode
Get example
> get wl n i
R000014
192.168.0.79
wlan.network.netmask
Abbreviation
wl n n
Access
get
Description
Returns the wlan interface IPv4 netmask resolved by DHCP.
Note: To set a static netmask, use the wlan.static.netmask variable.
Arguments
-
Default
0.0.0.0
Properties
- available in Safe Mode
Get example
> get wl n n
R000015
255.255.255.0
wlan.network.status
Abbreviation
wl n s
Access
get
Description
Returns the wlan network status. 0 = down, 1 = WLAN connected, 2 = IP network connected (with a valid IP address)
Arguments
-
Default
0
Properties
- available in Safe Mode
Get example
> get wl n s
R000003
2
wlan.passkey
Abbreviation
wl p
Access
get/set
Description
The WPA passphrase, WPA PSK or WEP key used when connecting to a Wi-Fi Access Point.
Notes for WEP
- The WEP key is replicated across each of the four possible keys.
- Silabs STRONGLY discourages the use of WEP - it is NOT secure!
Arguments
<passphrase> / <WEP key> | Description |
---|---|
WPA Passphrase | length: 8 - 63 characters |
WPA PSK | length: 64 characters |
WEP Key | A 40-bit WEP key is specified as a 5-byte hex string, for example: 1122334455 A 104-bit WEP key is specified as 13-byte hex string, for example: 112233445566778899aabbccdd |
"" | Sets a NULL passphrase |
Default
""
Properties
- network_restart to apply change
- available in Safe Mode
- preserved by NVM Backup
Get example
> get wl p
R000000
Set example
> set wl p "Use the force!"
R000008
Set OK
wlan.rate.protocol
Abbreviation
wl r p
Access
get/set
Description
WLAN client data rate protocol selection.
Arguments
<11b/11g/11n/auto>
Value | Description |
---|---|
11b | Restrict 802.11 PHY data rates to 802.11b |
11g | Restrict 802.11 PHY data rates to 802.11g |
11n | Restrict 802.11 PHY data rates to 802.11n |
auto | Automatically select the best rate from all 802.11b/g/n rates |
Default
auto
Properties
- network_restart to apply change
- available in Safe Mode
- preserved by NVM Backup
Get example
> get wl r p
auto
Set example
> set wlan.rate.protocol 11b
Set OK
wlan.ssid
Abbreviation
wl s
Access
get/set
Description
The name of the AP the wlan client interface will attempt to join.
Arguments
<ssid>
Default
""
Properties
- network_restart to apply change
- available in Safe Mode
- preserved by NVM Backup
Get example
> get wl s
R000012
My Home AP
Set example
> set wl s "Obi-wan Kenobi"
R000008
Set OK
wlan.static.dns
Abbreviation
wl t d
Access
get/set
Description
DNS server address if static network settings are used for the wlan interface.
See Networking and Security, DNS Server.
Arguments
<[IP address]/[host name]>
Default
8.8.8.8
Properties
- network_restart to apply change
- available in Safe Mode
- preserved by NVM Backup
Get example
> get wl t d
R000009
8.8.8.8
Set example
> set wl t d 8.8.4.4
R000008
Set OK
wlan.static.gateway
Abbreviation
wl t g
Access
get/set
Description
Gateway address if static network settings are used for the wlan interface.
Arguments
<IP address>
Default
0.0.0.0
Properties
- network_restart to apply change
- available in Safe Mode
- preserved by NVM Backup
Get example
> get wl t g
R000009
0.0.0.0
Set example
> set wl t g 192.168.0.1
R000008
Set OK
wlan.static.ip
Abbreviation
wl t i
Access
get/set
Description
Local IP address if static network settings are used for the wlan interface.
Arguments
<IP address>
Default
0.0.0.0
Properties
- network_restart to apply change
- available in Safe Mode
- preserved by NVM Backup
Get example
> get wl t i
R000009
0.0.0.0
Set example
> set wl t i 192.168.0.2
R000008
Set OK
wlan.static.netmask
Abbreviation
wl t n
Access
get/set
Description
Netmask if static network settings are used for the wlan interface.
Arguments
<network mask>
Default
0.0.0.0
Properties
- network_restart to apply change
- available in Safe Mode
- preserved by NVM Backup
Get example
> get wl t n
R000009
0.0.0.0
Set example
> set wl t n 255.255.255.0
R000008
Set OK
wlan.tx_power
Abbreviation
wl t
Access
get/set
Description
The Wi-Fi RF transmit power in units of dBm. Range is 0-31. The maximum achievable transmit power is dependent on the capability of the module.
The maximum transmit power is module dependent. The limit is +18dBm for the AMW004, AMW006 and AMW106 modules in all regions.
Regulatory Compliance in Europe & Japan
In Europe and Japan, the antenna gain must be taken into account to limit transmit power to +18dBm. Antenna gain is subtracted from the maximum of +18dBm to calculate the value of wlan.tx_power
.
For a device with an internal antenna, the known antenna gain is programmed into the firmware, and is automatically subtracted by Gecko OS.
For a device with an external antenna, the antenna gain must be measured, and the maximum wlan.tx_power
value manually set to:
wlan.tx_power = 18 - antenna_gain
Arguments
0-31/auto
Default
auto
Properties
- available in Safe Mode
- preserved by NVM Backup
Get example
> get wl t
R000006
auto
Set example
> set wl t 15
R000008
Set OK