Power Manager
Description
Power Manager.
Initialization
The power manager must be initialized prior to any call to power manager API. If sl_system is used, only sl_system_init() must be called, otherwise sl_power_manager_init() must be called manually. Note that the power manager must be initialized after the clock(s), when initialized manually, as the power manager check which oscillators are used during the initialization phase.
Add and remove requirements
The drivers should add and remove energy mode requirements, at runtime, on the lowest energy mode for them depending on their state. When calling sl_power_manager_sleep(), the lowest possible Energy mode will be automatically selected.
It is possible to add and remove requirements from ISR. If a specific energy mode is required in the ISR, but not required to generate the interrupt, a requirement on the energy mode can be added from the ISR. It is guaranteed that the associated clock will be active once sl_power_manager_add_requirement() returns. The EM requirement can be also be removed from an ISR.
Subscribe to events
It possible to get notified when the system transition from a power level to another power level. This can allow to do some operations depending on which level the system goes, such as saving/restoring context.
Sleep
When the software has no more operation and only need to wait for an event, the software must call sl_power_manager_sleep(). This is automatically done when the kernel is present, but it needs to be called from the super loop in a baremetal project.
Query callback functions
Is OK to sleep
Between the time sl_power_manager_sleep
is called and the MCU is really put in a lower Energy mode, it is possible that an ISR occur and require the system to resume at that time instead of sleeping. So a callback is called in a critical section to validate that the MCU can go to sleep.
In case of an application that runs on an RTOS, the RTOS will take care of determining if it is ok to sleep. In case of a baremetal application, the function sl_power_manager_is_ok_to_sleep()
will be generated automatically by Simplicity Studio's wizard. The function will look at multiple software modules from the SDK to take a decision. The application can contribute to the decision by defining the function app_is_ok_to_sleep()
. If any of the software modules (including the application via app_is_ok_to_sleep()
) return false, the process of entering in sleep will be aborted.
Sleep on ISR exit
When the system enters sleep, the only way to wake it up is via an interrupt or exception. By default, the power manager will assume that when an interrupt occurs and the corresponding ISR has been executed, the system must not go back to sleep. However, in the case where all the processing related to this interrupt is performed in the ISR, it is possible to go back to sleep by using this hook.
In case of an application that runs on an RTOS, the RTOS will take care of determining if the system can go back to sleep on ISR exit. The power manager will ensure the system resumes its operations as soon as a task is resumed, posted or that its delay expires. In case of a baremetal application, the function sl_power_manager_sleep_on_isr_exit()
will be generated automatically by Simplicity Studio's wizard. The function will look at multiple software modules from the SDK to take a decision. The application can contribute to the decision by defining the function app_sleep_on_isr_exit()
. The generated function will take a decision based on the value returned by the different software modules (including the application via app_sleep_on_isr_exit()
):
SL_POWER_MANAGER_IGNORE
: if the software module did not cause the system wakeup and/or doesn't want to contribute to the decision. SL_POWER_MANAGER_SLEEP
: if the software module did cause the system wakeup, but the system should go back to sleep. SL_POWER_MANAGER_WAKEUP
: if the software module did cause the system wakeup, and the system should not go back to sleep.
If any software module returned SL_POWER_MANAGER_SLEEP
and none returned SL_POWER_MANAGER_WAKEUP
, the system will go back to sleep. Any other combination will cause the system not to go back to sleep.
Debugging feature
By setting the configuration define SL_POWER_MANAGER_DEBUG to 1, it is possible to record the requirements currently set and their owner. It is possible to print at any time a table that lists all the added requirements and their owner. This table can be printed by caling the function sl_power_manager_debug_print_em_requirements(). Make sure to add the following define
to any application code source file that adds and removes requirements.
Usage Example
Data Structures | |
struct | sl_power_manager_em_transition_event_info_t |
TODO. | |
struct | sl_power_manager_em_transition_event_handle_t |
TODO. | |
Functions | |
sl_status_t | sl_power_manager_init (void) |
Initialize Power Manager module. | |
void | sl_power_manager_sleep (void) |
Sleep at the lowest allowed energy mode. | |
void | sl_power_manager_add_em_requirement (sl_power_manager_em_t em) |
Adds requirement on given energy mode. | |
void | sl_power_manager_remove_em_requirement (sl_power_manager_em_t em) |
Removes requirement on given energy mode. | |
void | sl_power_manager_subscribe_em_transition_event (sl_power_manager_em_transition_event_handle_t *event_handle, const sl_power_manager_em_transition_event_info_t *event_info) |
Registers a callback to be called on given Energy Mode transition(s). | |
void | sl_power_manager_unsubscribe_em_transition_event (sl_power_manager_em_transition_event_handle_t *event_handle) |
Unregisters an event callback handle on Energy mode transition. | |
int32_t | sl_power_manager_schedule_wakeup_get_restore_overhead_tick (void) |
Get configurable overhead value for early restore time in Sleeptimer ticks when a schedule wake-up is set. | |
void | sl_power_manager_schedule_wakeup_set_restore_overhead_tick (int32_t overhead_tick) |
Set configurable overhead value for early restore time in Sleeptimer ticks used for schedule wake-up. | |
uint32_t | sl_power_manager_schedule_wakeup_get_minimum_offtime_tick (void) |
Get configurable minimum off-time value for schedule wake-up in Sleeptimer ticks. | |
void | sl_power_manager_schedule_wakeup_set_minimum_offtime_tick (uint32_t minimum_offtime_tick) |
Set configurable minimum off-time value for schedule wake-up in Sleeptimer ticks. | |
void | sl_power_manager_debug_print_em_requirements (void) |
Print a table that describes the current requirements on each energy mode and their owner. | |
Typedefs | |
typedef uint32_t | sl_power_manager_em_transition_event_t |
Mask of all the event(s) to listen to. | |
typedef void(* | sl_power_manager_em_transition_on_event_t) (sl_power_manager_em_t from, sl_power_manager_em_t to) |
Typedef for the user supplied callback function which is called when an energy mode transition occurs. | |
Enumerations | |
enum | sl_power_manager_em_t { SL_POWER_MANAGER_EM0 = 0, SL_POWER_MANAGER_EM1, SL_POWER_MANAGER_EM2, SL_POWER_MANAGER_EM3, SL_POWER_MANAGER_EM4 } |
Energy modes. | |
enum | sl_power_manager_on_isr_exit_t { SL_POWER_MANAGER_IGNORE = (1UL << 0UL), SL_POWER_MANAGER_SLEEP = (1UL << 1UL), SL_POWER_MANAGER_WAKEUP = (1UL << 2UL) } |
On ISR Exit Hook answer. | |
Function Documentation
◆ sl_power_manager_init()
sl_status_t sl_power_manager_init | ( | void |
| ) |
Initialize Power Manager module.
- Returns
- Status code
◆ sl_power_manager_sleep()
void sl_power_manager_sleep | ( | void |
| ) |
Sleep at the lowest allowed energy mode.
- Note
- Must not be called from ISR
- Note
- This function will expect and call a callback with the following signature:
bool sl_power_manager_is_ok_to_sleep(void)
- This function can be used to cancel a sleep action and handle the possible race condition where an ISR that would cause a wakeup is triggered right after the decision to call sl_power_manager_sleep() has been made.
Usage example:
◆ sl_power_manager_add_em_requirement()
|
inline |
Adds requirement on given energy mode.
- Parameters
-
em
Energy mode to add the requirement to:
◆ sl_power_manager_remove_em_requirement()
|
inline |
Removes requirement on given energy mode.
- Parameters
-
em
Energy mode to remove the requirement to:
◆ sl_power_manager_subscribe_em_transition_event()
void sl_power_manager_subscribe_em_transition_event | ( | sl_power_manager_em_transition_event_handle_t * | event_handle, |
const sl_power_manager_em_transition_event_info_t * | event_info |
||
) |
Registers a callback to be called on given Energy Mode transition(s).
- Parameters
-
event_handle
Event handle (no initialization needed). event_info
Event info structure that contains the event mask and the callback that must be called.
- Note
- Adding and removing requirement(s) from a callback on a transition event is not supported.
- The parameters passed must be persistent, meaning that they need to survive until the callback fires.
Usage example:
◆ sl_power_manager_unsubscribe_em_transition_event()
void sl_power_manager_unsubscribe_em_transition_event | ( | sl_power_manager_em_transition_event_handle_t * | event_handle | ) |
Unregisters an event callback handle on Energy mode transition.
- Parameters
-
event_handle
Event handle which must be unregistered (must have been registered previously).
- Note
- An EFM_ASSERT is thrown if the handle is not found.
◆ sl_power_manager_schedule_wakeup_get_restore_overhead_tick()
int32_t sl_power_manager_schedule_wakeup_get_restore_overhead_tick | ( | void |
| ) |
Get configurable overhead value for early restore time in Sleeptimer ticks when a schedule wake-up is set.
- Returns
- Current overhead value for early restore time.
◆ sl_power_manager_schedule_wakeup_set_restore_overhead_tick()
void sl_power_manager_schedule_wakeup_set_restore_overhead_tick | ( | int32_t | overhead_tick | ) |
Set configurable overhead value for early restore time in Sleeptimer ticks used for schedule wake-up.
Must be called after initialization else the value will be overwritten.
- Parameters
-
overhead_tick
Overhead value to set for early restore time.
- Note
- The overhead value can also be negative to remove time from the restore process.
◆ sl_power_manager_schedule_wakeup_get_minimum_offtime_tick()
uint32_t sl_power_manager_schedule_wakeup_get_minimum_offtime_tick | ( | void |
| ) |
Get configurable minimum off-time value for schedule wake-up in Sleeptimer ticks.
- Returns
- Current minimum off-time value for schedule wake-up.
- Note
- Turning on external high frequency clock, such as HFXO, requires more energy since we must supply higher current for the wake-up. Therefore, when an 'external high frequency clock enable' is scheduled in 'x' time, there is a threshold 'x' value where turning off the clock is not worthwhile since the energy consumed by taking into account the wake-up will be greater than if we just keep the clock on until the next scheduled clock enabled. This threshold value is what we refer as the minimum off-time.
◆ sl_power_manager_schedule_wakeup_set_minimum_offtime_tick()
void sl_power_manager_schedule_wakeup_set_minimum_offtime_tick | ( | uint32_t | minimum_offtime_tick | ) |
Set configurable minimum off-time value for schedule wake-up in Sleeptimer ticks.
- Parameters
-
minimum_offtime_tick
minimum off-time value to set for schedule wake-up.
- Note
- Turning on external high frequency clock, such as HFXO, requires more energy since we must supply higher current for the wake-up. Therefore, when an 'external high frequency clock enable' is scheduled in 'x' time, there is a threshold 'x' value where turning off the clock is not worthwhile since the energy consumed by taking into account the wake-up will be greater than if we just keep the clock on until the next scheduled clock enabled. This threshold value is what we refer as the minimum off-time.
◆ sl_power_manager_debug_print_em_requirements()
void sl_power_manager_debug_print_em_requirements | ( | void |
| ) |
Print a table that describes the current requirements on each energy mode and their owner.
Typedef Documentation
◆ sl_power_manager_em_transition_event_t
typedef uint32_t sl_power_manager_em_transition_event_t |
Mask of all the event(s) to listen to.
◆ sl_power_manager_em_transition_on_event_t
typedef void(* sl_power_manager_em_transition_on_event_t) (sl_power_manager_em_t from, sl_power_manager_em_t to) |
Typedef for the user supplied callback function which is called when an energy mode transition occurs.
- Parameters
-
from
Energy mode we are leaving. to
Energy mode we are entering.
Enumeration Type Documentation
◆ sl_power_manager_em_t
◆ sl_power_manager_on_isr_exit_t
On ISR Exit Hook answer.