Atomic Operations

Description

Atomic operations.

Macros

#define sl_atomic_load(dest, source)   ((dest) = (source))
 Perform an atomic load.
 
#define sl_atomic_store(dest, source)   ((dest) = (source))
 Perform an atomic store.
 

Macro Definition Documentation

◆ sl_atomic_load

#define sl_atomic_load (   dest,
  source 
)    ((dest) = (source))

Perform an atomic load.

Use when a variable must be read from RAM.

Parameters
destVariable where to copy the loaded value.
sourceVariable from where to load the value.
Note
Does only support native types <= 32 bits.
Load operation on 32 bit value is atomic on ARM architecture.

◆ sl_atomic_store

#define sl_atomic_store (   dest,
  source 
)    ((dest) = (source))

Perform an atomic store.

Use when a value must be stored in RAM.

Parameters
destVariable where to store the value.
sourceVariable that contains the value to store in 'dest'.
Note
Does only support native types <= 32 bits.
Store operation on 32 bit value is atomic on ARM architecture.