sl_se_cert_size_type_t Struct Reference

Certificate size data structure.

#include <sl_se_manager_types.h>

Data Fields

uint32_t batch_id_size
 size in bytes of the Batch certificate
 
uint32_t se_id_size
 size in bytes of the SE ID certificate
 
uint32_t host_id_size
 size in bytes of the Host ID certificate
 

Certificate size data structure.

Field Documentation

◆ batch_id_size

uint32_t sl_se_cert_size_type_t::batch_id_size

size in bytes of the Batch certificate

◆ se_id_size

uint32_t sl_se_cert_size_type_t::se_id_size

size in bytes of the SE ID certificate

◆ host_id_size

uint32_t sl_se_cert_size_type_t::host_id_size

size in bytes of the Host ID certificate