Atomic Operations
Description
Atomic operations.
Macros | |
#define | sl_atomic_load(dest, source) ((dest) = (source)) |
Perform an atomic load. | |
#define | sl_atomic_store(dest, source) ((dest) = (source)) |
Perform an atomic store. | |
Macro Definition Documentation
◆ sl_atomic_load
#define sl_atomic_load | ( | dest, |
|
source |
|||
) | ((dest) = (source)) |
Perform an atomic load.
Use when a variable must be read from RAM.
- Parameters
-
dest
Variable where to copy the loaded value. source
Variable from where to load the value.
- Note
- Does only support native types <= 32 bits.
- Load operation on 32 bit value is atomic on ARM architecture.
◆ sl_atomic_store
#define sl_atomic_store | ( | dest, |
|
source |
|||
) | ((dest) = (source)) |
Perform an atomic store.
Use when a value must be stored in RAM.
- Parameters
-
dest
Variable where to store the value. source
Variable that contains the value to store in 'dest'.
- Note
- Does only support native types <= 32 bits.
- Store operation on 32 bit value is atomic on ARM architecture.