Legacy HAL
Description
Legacy HAL API.
Modules | |
Application Bootloader Interface | |
Definition of the application bootloader interface. | |
Common Bootloader | |
Common bootloader interface defines and functions. | |
Cyclic Redundancy Check | |
Functions that provide access to cyclic redundancy code (CRC) calculation. See crc.h for source code. | |
Diagnostics | |
Crash and watchdog diagnostic functions. | |
Microcontroller functions | |
Microcontroller functions. | |
Random Numbers | |
Functions that provide access to random numbers. | |
Reset Cause Definitions | |
Definitions for all the reset cause types. | |
SimEE2 to NVM3 Upgrade | |
Simulated EEPROM 1 and 2 | |
Simulated EEPROM 1 and 2 legacy storage. | |
Standalone Bootloader | |
Definition of the standalone bootloader interface. | |
Macros | |
#define | simulatedTimePasses() |