Command Line Interface
Description
Command Line Interface (CLI)
Introduction
The Command Line Interface (CLI) software component simplifies creating command line user interfaces for programs. It handles tasks such as receiving keyboard input, parsing the input strings for commands and arguments, and finally call the proper C function with decoded and validated arguments. Functions can use standard output functions such as printf to write information to the console.
Multiple components (parts of an application) may define CLI commands where the running program will typically merge all commands into a super-set of commands with common input and output, I/O. The CLI uses I/O functions provided by the I/O Streams framework, iostream.
The CLI component supports multiple instances where separate CLI instances will use separate iostream instances. Groups of commands can be assigned to specific CLI instances, making it possible for one application to use multiple CLI instances where each is customized for its particular use.
Content
Features Design Configuration Examples Extensions
Features
The CLI has several built in features that will be inherited by all applications using the CLI component. The following sections will explain some of the CLI features.
Please note:** Some of the features can be simplified or removed to reduce code size by changing the configuration of the application.
Command Groups
The CLI support both stand alone commands and commands that belong to groups. A stand alone command is executed by typing just the command name and arguments. If a command belong to a group, the group name must be typed before the command name. Groups can be nested, and in that case, all group names must be typed before the command name.
If an application has implemented the commands on
and off
that are part of the groups green
and red
in group led
, the user can type: led green on
or led red off
to control the LEDs.
Help
The CLI has a built in help command, which can be used as follows:
By typing help
, all commands are listed.
By typing help group
, all commands in the group
are listed.
By typing help command
, help for the command
is shown.
The information that is displayed when using the help
command must be supplied by the implementer. Details for each command must be placed in command tables. See the Command tables section for more details.
Auto-Complete
The CLI can complete a partially typed command by pressing the TAB key.
Cursor Movement
The up-arrow and down-arrow keys can be used to navigate up and down in the history buffer.
The left-arrow and right-arrow keys are used to move the cursor in the current command line. The BACKSPACE key is used to delete the character to the left of the cursor. The DEL key is used to delete the character under the cursor. Typed characters will be inserted at the cursor position.
Command History
Commands will be stored in the history buffer when executed. Previous commands can be executed again by pressing the up-arrow key one or more times.
Please note:** The history buffer is a simple character array, which does not define how many command lines can be stored. The history buffer will store command lines sequentially, making room for more short commands than long.
Dynamic registration of New Commands
An application using the CLI component can define commands that must be installed either at compile time or at run time. Defining commands at compile time may be sufficient for simple applications, while more advanced applications with several CLI instances, may utilize that the CLI can add command groups at run time.
Central decoding and validation of command arguments
The CLI has built in functions to decode and validate command arguments. The command handler will not be called unless the command is entered with correct arguments.
The CLI argument validation can handle signed and unsigned numeric values with 8, 16 and 32 bit sizes, hexadecimal and string arguments. The command handler will be called with decoded arguments using an arc, argv
pattern similar to how C/C++ applications pass command line arguments to the main function.
If none of the built in argument types can be used by the command, it can use string arguments and decode the strings in the command handler.
Please note:** For the last argument, it is possible to specify that it is optional, mandatory or can have multiple values.
Input and output
The CLI is using iostreams for input and output. Each CLI instance must have a dedicated iostream instance.
Assigning an iostream instance to a CLI instance is usually done with an application configuration. If the application has only one CLI and one iostream instance, the configuration will automatically assign the iostream instance to the CLI instance.
Requirements not defined by the CLI
Command naming rules or output formats are not defined by the CLI.
Design
To fully understand how to use the CLI, it is crucial to understand the design and some implementation deatils. The following sections will try to explain the basics and how to create user commands.
Modules
The CLI has been implementated as two independent software modules; input handler
and command interpreter
. The input handler
handles the user input and allows the user to enter command lines. When the user type the ENTER key, the input string is passed to the command interpreter
where the string will be interpreted and the appropriate command handler will be called with the command arguments.
Normally both modules are used together, but an application can use the command interpreter
directly. In that case, the command interpreter
must be called with a command line as input parameter.
Command signature
All command handlers must have the same signature, defined in sl_cli_types.h
:
Command arguments
Command arguments are available via the arguments pointer passed to the command handler function.
The arguments pointer will point to a struct holding the actual argument values.
The arguments struct has the following definition:
The handle
identifies the CLI instance where the command was issued. By including the instance handle, it is possible to share the same command handler between multiple CLI instances.
By using the argc
, argv
way of passing argument values, it is possible to have a common command handler signature but support variable number of arguments.
When the command handler is called, the argc
, argv
arguments will contain all commands and arguments. Because the CLI supports command groups, the command may consist of multiple command groups along with the command itself. The arg_ofs
tells the command handler the offset where the command arguments begin.
The cli.h has defined the following macros that can be used to get argument values. The macros use a
for the arguments pointer and n
for the argument offset, starting on 0 for the first argument.
Command tables
Adding commands to the CLI requires use of three different data structures. The data structures have a root node referred to as a "command group", where sub-structures defining command details are nested. The "command group" may contain details for one or more commands, and it is possible to install multiple "command groups" in each CLI instance.
The "command group" must be of the type:
Please note:** Each time a command group shall be installed in a CLI instance, the application must support one unique command group data structure. Command groups cannot be re-used or shared between CLI instances.
The next level is an array where each of the elements must be a "command entry". There will typically be one array element for each command. If a command has both a long and a short (shortcut) name, it will take two array elements.
Each of the "command entries" must be of the type:
A "command entries" array can be re-used and shared between multiple CLI instances.
And finally "command information" for commands are defined in one data structure for each command. The "command information" structure is defined with the type:
A "command information" data structure can be re-used and shared between multiple CLI commands and instances.
Command handler
In addition to the tables described above, each command must have a command handler. The command handler is typically written in C-code, and all command handlers have the same signature. The command handler function prototype has the following defition:
Differences between bare-metal and kernel configurations
The CLI component can be used in both bare-metal and kernel configurations. There are some differences between the two configurations that is explained in the following sections.
Bare-metal
In a bare-metal configuraton, the input handler
has a process-action (tick) function that will poll the iostream for input. When generating a project with uc, the CLI process-action function will be installed into the system framework. Calling the sl_system_process_action
function will call the CLI process-action function.
Please note: Cli command handlers that take a long time to execute can (should) return from the process-action function before they are complete to not stall other component process-action functions. Execution will in that case be split into several calls to the process-action function. The application should not make any assumptions about when any of the command handlers have completed execution based on when the sl_system_process_action
returns.
Kernel
In a kernel configuration, the CLI will create a task where the input handler
will poll the iostream for input data. There will be created one task for each CLI instance, and the task(s) must be started by the application by calling the sl_system_kernel_start
function.
Configuration
The CLI has two sets of configurations. One is common for all CLI instances and is placed in the sl_cli_config.h
file. The other is a configuration file for each CLI instance with the file name sl_cli_config_<instance-name>.h
.
Examples
The following steps demonstrates how to create and install a CLI command.
Please note: To avoid forward definitions in the C-code, the following steps will typically be implemented in reverse order.
Include the cli
and iostream
components to the project. Both cli
and iostream_usart
instances must specify instance names. The iostream_usart
component has some pre-defined instance names while the cli
instance name can be anything.
Create the command group at the top level:
Create the array of commands, containing two elements in this example:
Create command details for the two commands:
Create command handlers for the two commands:
And finally call the function to install the commands.
The output from executing help
will in this case be:
Extensions
The CLI comes with some pre-made components that can be useful for some applications. To take advantage of these components, the user must:
- Define the command(s) in the command tables. Use the command handlers supplied with the component(s).
- Include the component(s) in the project.
The components come with the command handlers and do all the necessary integration with the CLI. The componentes do however not define the command name, it must be defined by the application implementer.
Please note:** The CLI extensions described here will use the method of splitting some of the command handler operations into multiple process-action calls for bare-metal configuration.
Common properties for the storage components:** The storage components share some common properties although data is stored in different locations. The most important are: New commands can be added, existing commands can be deleted and stored commands can be executed.
One benefit of running commands from a storage compared to typing the commands at user input is that the next command in the list will be executed immediately after the previous command has completed. Commands will be executed in the sequence they are added and stored, and there will be zero or little delay between commands.
CLI Storage NVM3
The cli_storage_nvm3
component has been designed to store command lines in NVM3 storage. In addition to let the user control when the commands are executed, the stored commands will automatically be executed at program start.
The cli_storage_nvm3
component does not define the user commands, but it implements a few functions where the following four are designed to be used as CLI command handlers directly.
In addition, it is possible to get the number of command lines stored in NVM3 storage by calling:
The cli_storage_nvm3
depends on the cli_default
component that defines the NVM3 storage area. This area is typically shared between different parts of the application, where each has its own range of NVM3 object keys to avoid collisions. The cli_storage_nvm3
component has got a range with 256 keys.
It is possible to configure each CLI instance to use a sub-set of the available 256 keys to separate commands between different CLI instances.
CLI Storage RAM
The cli_storage_ram
component has been designed to store command lines in a ram buffer.
The cli_storage_ram
component does not define the user commands, but it implements a few functions where the following four are designed to be used as CLI command handlers directly.
In addition, it is possible to get the number of command lines stored in RAM by calling:
Each instance of the CLI will have its own RAM buffer. Commands defined in one CLI instance will not be available for other instances.
CLI Delay
The cli_delay
component may be useful to add delays between commands when running command sequences from a storage. The function will delay for the specified number of milliseconds. During the delay, it will allow other components to run in the background.
The command handler has the following function prototype:
Modules | |
CLI Commands in NVM3 | |
Support for CLI commands stored in and executed from NVM3. | |
CLI Commands in RAM | |
Support for CLI commands stored in and executed from RAM. | |
CLI Delay | |
CLI Delay. | |
Functions | |
uint8_t * | sl_cli_get_argument_hex (sl_cli_command_arg_t *a, size_t n, size_t *l) |
Get the hex argument length and value. | |
void | sl_cli_clear (sl_cli_handle_t handle) |
Clear (reset) a CLI. | |
void | sl_cli_redirect_command (sl_cli_handle_t handle, sl_cli_command_function_t command_function, const char *prompt, void *aux) |
Redirect user input. | |
sl_status_t | sl_cli_handle_input (sl_cli_handle_t handle, char *string) |
Handle input. | |
sl_status_t | sl_cli_instance_init (sl_cli_handle_t handle, sl_cli_instance_parameters_t *parameters) |
Initialize a CLI instance. | |
bool | sl_cli_is_ok_to_sleep (sl_cli_handle_t handle) |
Check if the CLI instance can allow sleep. | |
void | sl_cli_tick_instance (sl_cli_handle_t handle) |
The bare metal tick function. | |
bool | sl_cli_input_char (sl_cli_handle_t handle, char c) |
Handle new input char from the terminal, both in terms of writing back to terminal and writing to the input buffer. | |
void | sl_cli_input_clear (sl_cli_handle_t handle) |
Empty the input buffer. | |
sl_status_t | sl_cli_tokenize (char input[], int *token_c, char *token_v[]) |
Split a C-string on space, ignoring sections in {} or "". | |
bool | sl_cli_command_add_command_group (sl_cli_handle_t handle, sl_cli_command_group_t *command_group) |
Add a new command group. | |
bool | sl_cli_command_remove_command_group (sl_cli_handle_t handle, sl_cli_command_group_t *command_group) |
Remove a command group. | |
const sl_cli_command_entry_t * | sl_cli_command_find (sl_cli_handle_t handle, int *token_c, char *token_v[], int *arg_ofs, bool *single_flag, bool *help_flag) |
Find a command given the command groups and input arguments. | |
sl_status_t | sl_cli_command_execute (sl_cli_handle_t handle, char *input) |
Find and execute a command given the string input and the command table. | |
Macros | |
#define | sl_cli_get_argument_count(a) ((int)(a->argc - a->arg_ofs)) |
Obtain the number of command arguments. | |
#define | sl_cli_get_argument_int8(a, n) (*(int8_t *)(a->argv[a->arg_ofs + n])) |
Obtain int8 arguments. | |
#define | sl_cli_get_argument_int16(a, n) (*(int16_t *)(a->argv[a->arg_ofs + n])) |
Obtain int16 arguments. | |
#define | sl_cli_get_argument_int32(a, n) (*(int32_t *)(a->argv[a->arg_ofs + n])) |
Obtain int32 arguments. | |
#define | sl_cli_get_argument_uint8(a, n) (*(uint8_t *)(a->argv[a->arg_ofs + n])) |
Obtain uint8 arguments. | |
#define | sl_cli_get_argument_uint16(a, n) (*(uint16_t *)(a->argv[a->arg_ofs + n])) |
Obtain uint16 arguments. | |
#define | sl_cli_get_argument_uint32(a, n) (*(uint32_t *)(a->argv[a->arg_ofs + n])) |
Obtain uint32 arguments. | |
#define | sl_cli_get_argument_string(a, n) ((char *)(a->argv[a->arg_ofs + n])) |
Obtain string arguments. | |
#define | sl_cli_get_command_count(a) ((int)(a->arg_ofs)) |
Obtain the number of command strings. | |
#define | sl_cli_get_command_string(a, n) ((char *)(a->argv[n])) |
Obtain the command string(s). | |
#define | SL_CLI_INPUT_DIRECTION_UP (1) |
MACROS ************************************. | |
#define | SL_CLI_INPUT_DIRECTION_DOWN (-1) |
Define the DOWN-direction. | |
#define | SL_CLI_ARG_UINT8 (0x00U) |
UINT8 argument type. | |
#define | SL_CLI_ARG_UINT16 (0x01U) |
UINT16 argument type. | |
#define | SL_CLI_ARG_UINT32 (0x02U) |
UINT32 argument type. | |
#define | SL_CLI_ARG_INT8 (0x03U) |
INT8 argument type. | |
#define | SL_CLI_ARG_INT16 (0x04U) |
INT16 argument type. | |
#define | SL_CLI_ARG_INT32 (0x05U) |
INT32 argument type. | |
#define | SL_CLI_ARG_STRING (0x06U) |
STRING argument type. | |
#define | SL_CLI_ARG_HEX (0x07U) |
HEX argument type. | |
#define | SL_CLI_ARG_UINT8OPT (0x10U) |
Optional UINT8 argument type. | |
#define | SL_CLI_ARG_UINT16OPT (0x11U) |
Optional UINT16 argument type. | |
#define | SL_CLI_ARG_UINT32OPT (0x12U) |
Optional UINT32 argument type. | |
#define | SL_CLI_ARG_INT8OPT (0x13U) |
Optional INT8 argument type. | |
#define | SL_CLI_ARG_INT16OPT (0x14U) |
Optional INT16 argument type. | |
#define | SL_CLI_ARG_INT32OPT (0x15U) |
Optional INT32 argument type. | |
#define | SL_CLI_ARG_STRINGOPT (0x16U) |
Optional STRING argument type. | |
#define | SL_CLI_ARG_HEXOPT (0x17U) |
Optional HEX argument type. | |
#define | SL_CLI_ARG_ADDITIONAL (0x20U) |
ADDITIONAL argument type. | |
#define | SL_CLI_ARG_WILDCARD (0x21U) |
WILDCARD argument type. | |
#define | SL_CLI_ARG_GROUP (0xFEU) |
GROUP argument type. | |
#define | SL_CLI_ARG_END (0xFFU) |
END argument type. | |
#define | SL_CLI_COMMAND(function, help_text, arg_help, ...) |
A macro, which is used to create commands. | |
#define | SL_CLI_COMMAND_GROUP(group_table, help_text) |
A macro, which is used to create command groups. | |
Variables | |
sl_cli_handle_t | sl_cli_default_handle |
The default CLI handle. | |
sl_cli_command_group_t * | sl_cli_default_command_group |
The default CLI command group. | |
Function Documentation
◆ sl_cli_get_argument_hex()
uint8_t* sl_cli_get_argument_hex | ( | sl_cli_command_arg_t * | a, |
size_t | n, |
||
size_t * | l |
||
) |
Get the hex argument length and value.
- Parameters
-
[in] a
A pointer to the command arguments. [in] n
The argument number. The first argument is number 0, the next 1, etc. [in] l
A pointer to the variable that receives the argument value length. Note: The length is stored in a 2 byte variable. Valid lengths are in the range 0 .. 65535.
- Returns
- A pointer to the value buffer.
◆ sl_cli_clear()
void sl_cli_clear | ( | sl_cli_handle_t | handle | ) |
Clear (reset) a CLI.
- Parameters
-
[in] handle
A handle to the CLI that will be cleared.
◆ sl_cli_redirect_command()
void sl_cli_redirect_command | ( | sl_cli_handle_t | handle, |
sl_cli_command_function_t | command_function, |
||
const char * | prompt, |
||
void * | aux |
||
) |
Redirect user input.
Normally, an input string is passed to the CLI command handler for execution, but with the redirect function the input string will be passed to the alternative function. If the alternative input function should not to be used, this function can be called with NULL in the command_function, prompt and aux.
- Parameters
-
[in] handle
A handle to the CLI. [in] command_function
A pointer to the function that will receive user input when the re-direct is active. NULL to stop the redirect. [in] prompt
A pointer to a string that will be used as command prompt in the redirect function. NULL to stop the redirect. [in] aux
A pointer that will be added to the redirect function arguments. NULL to stop the redirect.
◆ sl_cli_handle_input()
sl_status_t sl_cli_handle_input | ( | sl_cli_handle_t | handle, |
char * | string |
||
) |
Handle input.
Execute a complete command line with command and arguments.
- Parameters
-
[in] handle
A handle to the CLI. [in] string
A pointer to the string containing the command line that shall be executed.
- Returns
- Execution status. Note: If the command is redirected, the function will always return SL_STATUS_OK.
◆ sl_cli_instance_init()
sl_status_t sl_cli_instance_init | ( | sl_cli_handle_t | handle, |
sl_cli_instance_parameters_t * | parameters |
||
) |
Initialize a CLI instance.
- Parameters
-
[in] handle
A handle to the CLI. [in] parameters
A pointer to the structure containing instance parameters.
- Returns
- Initialization status.
◆ sl_cli_is_ok_to_sleep()
bool sl_cli_is_ok_to_sleep | ( | sl_cli_handle_t | handle | ) |
Check if the CLI instance can allow sleep.
This function is available in a bare metal configuration only.
- Parameters
-
[in] handle
A handle to the CLI instance.
- Returns
- A boolean that is true if the CLI allows sleep, else false.
◆ sl_cli_tick_instance()
void sl_cli_tick_instance | ( | sl_cli_handle_t | handle | ) |
The bare metal tick function.
- Parameters
-
[in] handle
A handle to the CLI instance.
◆ sl_cli_input_char()
bool sl_cli_input_char | ( | sl_cli_handle_t | handle, |
char | c |
||
) |
Handle new input char from the terminal, both in terms of writing back to terminal and writing to the input buffer.
This function should be called every time new input is detected. The behavior of the function is highly configurable through settings in cli_config.h.
- Parameters
-
[in,out] handle
A handle to a CLI instance. [in] c
Input char to be processed by the function.
- Returns
- Returns true if newline or return is detected, false otherwise.
◆ sl_cli_input_clear()
void sl_cli_input_clear | ( | sl_cli_handle_t | handle | ) |
Empty the input buffer.
This function should be called after newline has been detected and the information in the buffer has been processed.
- Parameters
-
[in,out] handle
A handle to a CLI instance.
◆ sl_cli_tokenize()
sl_status_t sl_cli_tokenize | ( | char | input[], |
int * | token_c, |
||
char * | token_v[] |
||
) |
Split a C-string on space, ignoring sections in {} or "".
- Note
- This function modifies the content of the input string, and points the pointers in tokens to addresses in the input string. In quote strings ("") or curly braces ({}), the string will not be split, The quotes will be removed, but curly braces are kept for validation. To avoid '"' being interpreted as start/end of quote string, it may be escaped using '\"', both within and outside of "...". '{' may be escaped using * '\{'. There is no need for escaping '}', since only hex digits are allowed within {...}. Backslash also needs be be escaped, as '\'.
- Parameters
-
[in,out] input
The C-string to be split. Must be '\0'-terminated. Will be modified, even if an error occurs. [out] token_c
The number of tokens put in the token_v array. [out] token_v
An array containing the tokens obtained from splitting.
- Returns
- Status of the operation.
◆ sl_cli_command_add_command_group()
bool sl_cli_command_add_command_group | ( | sl_cli_handle_t | handle, |
sl_cli_command_group_t * | command_group |
||
) |
Add a new command group.
- Parameters
-
[in,out] handle
A handle to a CLI instance. [in] command_group
A pointer to a command group structure. Note that the structure must initially have NULL in all elements except the command_table.
- Returns
- Returns true if the command_group could be added, false otherwise.
◆ sl_cli_command_remove_command_group()
bool sl_cli_command_remove_command_group | ( | sl_cli_handle_t | handle, |
sl_cli_command_group_t * | command_group |
||
) |
Remove a command group.
- Parameters
-
[in,out] handle
A handle to a CLI instance. [in] command_group
A pointer to a command group structure.
- Returns
- Returns true if the command_group could be removed, false otherwise.
◆ sl_cli_command_find()
const sl_cli_command_entry_t* sl_cli_command_find | ( | sl_cli_handle_t | handle, |
int * | token_c, |
||
char * | token_v[], |
||
int * | arg_ofs, |
||
bool * | single_flag, |
||
bool * | help_flag |
||
) |
Find a command given the command groups and input arguments.
- Parameters
-
[in,out] handle
A handle to a CLI instance. [in] token_c
A number of arguments given. [in] token_v
An array containing the token_v obtained from tokenization. [out] arg_ofs
An integer that will get the index to the first command argument. Whether the command is in a group or not will affect the arg_ofs value. [out] single_flag
Boolean that is set to true if a specific command is detected. For help, the function may return a pointer to a command entry table or NULL, and in these cases the single_flag is set to false. [out] help_flag
Boolean that is set to true if "help" is detected, else set to false.
- Returns
- A pointer to a command entry for the given command. If the command is not found, the returned value can be NULL. If a help command is issued, the returned value may point to a command entry table.
◆ sl_cli_command_execute()
sl_status_t sl_cli_command_execute | ( | sl_cli_handle_t | handle, |
char * | input |
||
) |
Find and execute a command given the string input and the command table.
- Note
- The input string will be modified in-place.
- Parameters
-
[in,out] handle
A handle to a CLI instance. [in,out] input
C-string containing the user input. Must be '\0'-terminated.
- Returns
- Status of the execution.
Macro Definition Documentation
◆ sl_cli_get_argument_count
#define sl_cli_get_argument_count | ( | a | ) | ((int)(a->argc - a->arg_ofs)) |
Obtain the number of command arguments.
Users obtain the number of command arguments with this macro.
- Parameters
-
[in] a
The number of command arguments.
- Returns
- The number of command arguments.
An example could be the CLI input of example_sub_menu example_command hello 255 -100 {AA BB CC}
with corresponding C code of: void example_command(sl_cli_command_arg_t *args) { // Get the number of arguments (after the command strings). int arg_count = sl_cli_get_argument_count(args); // arg_count = 4 }
◆ sl_cli_get_argument_int8
#define sl_cli_get_argument_int8 | ( | a, |
|
n |
|||
) | (*(int8_t *)(a->argv[a->arg_ofs + n])) |
Obtain int8 arguments.
- Parameters
-
[in] a
A pointer to the command arguments. [in] n
The argument number. The first argument is the number 0, the next 1, etc.
- Returns
- The argument value.
An example could be the CLI input of example_sub_menu example_command hello 255 -100 {AA BB CC}
with corresponding C code of: void example_command(sl_cli_command_arg_t *args) { // Get the arguments (after the command strings). char *text_ptr = sl_cli_get_argument_string(args, 0); // char ptr to // "hello" uint8_t num1_u8 = sl_cli_get_argument_uint8(args, 1); // num1_u8 = 255 int16_t num2_i16 = sl_cli_get_argument_int16(args, 2); // num2_i16 = -100 size_t hex_array_size; uint8_t *hex_array_ptr = sl_cli_get_argument_hex(args, 3, &hex_array_size); // uint8_t ptr to {0xAA, 0xBB, 0xCC}, hex_array_size = 3 }
◆ sl_cli_get_argument_int16
#define sl_cli_get_argument_int16 | ( | a, |
|
n |
|||
) | (*(int16_t *)(a->argv[a->arg_ofs + n])) |
Obtain int16 arguments.
- Parameters
-
[in] a
A pointer to the command arguments. [in] n
The argument number. The first argument is the number 0, the next 1, etc.
- Returns
- The argument value.
An example could be the CLI input of example_sub_menu example_command hello 255 -100 {AA BB CC}
with corresponding C code of: void example_command(sl_cli_command_arg_t *args) { // Get the arguments (after the command strings). char *text_ptr = sl_cli_get_argument_string(args, 0); // char ptr to // "hello" uint8_t num1_u8 = sl_cli_get_argument_uint8(args, 1); // num1_u8 = 255 int16_t num2_i16 = sl_cli_get_argument_int16(args, 2); // num2_i16 = -100 size_t hex_array_size; uint8_t *hex_array_ptr = sl_cli_get_argument_hex(args, 3, &hex_array_size); // uint8_t ptr to {0xAA, 0xBB, 0xCC}, hex_array_size = 3 }
◆ sl_cli_get_argument_int32
#define sl_cli_get_argument_int32 | ( | a, |
|
n |
|||
) | (*(int32_t *)(a->argv[a->arg_ofs + n])) |
Obtain int32 arguments.
- Parameters
-
[in] a
A pointer to the command arguments. [in] n
The argument number. The first argument is the number 0, the next 1, etc.
- Returns
- The argument value.
An example could be the CLI input of example_sub_menu example_command hello 255 -100 {AA BB CC}
with corresponding C code of: void example_command(sl_cli_command_arg_t *args) { // Get the arguments (after the command strings). char *text_ptr = sl_cli_get_argument_string(args, 0); // char ptr to // "hello" uint8_t num1_u8 = sl_cli_get_argument_uint8(args, 1); // num1_u8 = 255 int16_t num2_i16 = sl_cli_get_argument_int16(args, 2); // num2_i16 = -100 size_t hex_array_size; uint8_t *hex_array_ptr = sl_cli_get_argument_hex(args, 3, &hex_array_size); // uint8_t ptr to {0xAA, 0xBB, 0xCC}, hex_array_size = 3 }
◆ sl_cli_get_argument_uint8
#define sl_cli_get_argument_uint8 | ( | a, |
|
n |
|||
) | (*(uint8_t *)(a->argv[a->arg_ofs + n])) |
Obtain uint8 arguments.
- Parameters
-
[in] a
A pointer to the command arguments. [in] n
The argument number. The first argument is the number 0, the next 1, etc.
- Returns
- The argument value.
An example could be the CLI input of example_sub_menu example_command hello 255 -100 {AA BB CC}
with corresponding C code of: void example_command(sl_cli_command_arg_t *args) { // Get the arguments (after the command strings). char *text_ptr = sl_cli_get_argument_string(args, 0); // char ptr to // "hello" uint8_t num1_u8 = sl_cli_get_argument_uint8(args, 1); // num1_u8 = 255 int16_t num2_i16 = sl_cli_get_argument_int16(args, 2); // num2_i16 = -100 size_t hex_array_size; uint8_t *hex_array_ptr = sl_cli_get_argument_hex(args, 3, &hex_array_size); // uint8_t ptr to {0xAA, 0xBB, 0xCC}, hex_array_size = 3 }
◆ sl_cli_get_argument_uint16
#define sl_cli_get_argument_uint16 | ( | a, |
|
n |
|||
) | (*(uint16_t *)(a->argv[a->arg_ofs + n])) |
Obtain uint16 arguments.
- Parameters
-
[in] a
A pointer to the command arguments. [in] n
The argument number. The first argument is the number 0, the next 1, etc.
- Returns
- The argument value.
An example could be the CLI input of example_sub_menu example_command hello 255 -100 {AA BB CC}
with corresponding C code of: void example_command(sl_cli_command_arg_t *args) { // Get the arguments (after the command strings). char *text_ptr = sl_cli_get_argument_string(args, 0); // char ptr to // "hello" uint8_t num1_u8 = sl_cli_get_argument_uint8(args, 1); // num1_u8 = 255 int16_t num2_i16 = sl_cli_get_argument_int16(args, 2); // num2_i16 = -100 size_t hex_array_size; uint8_t *hex_array_ptr = sl_cli_get_argument_hex(args, 3, &hex_array_size); // uint8_t ptr to {0xAA, 0xBB, 0xCC}, hex_array_size = 3 }
◆ sl_cli_get_argument_uint32
#define sl_cli_get_argument_uint32 | ( | a, |
|
n |
|||
) | (*(uint32_t *)(a->argv[a->arg_ofs + n])) |
Obtain uint32 arguments.
- Parameters
-
[in] a
A pointer to the command arguments. [in] n
The argument number. The first argument is the number 0, the next 1, etc.
- Returns
- The argument value.
An example could be the CLI input of example_sub_menu example_command hello 255 -100 {AA BB CC}
with corresponding C code of: void example_command(sl_cli_command_arg_t *args) { // Get the arguments (after the command strings). char *text_ptr = sl_cli_get_argument_string(args, 0); // char ptr to // "hello" uint8_t num1_u8 = sl_cli_get_argument_uint8(args, 1); // num1_u8 = 255 int16_t num2_i16 = sl_cli_get_argument_int16(args, 2); // num2_i16 = -100 size_t hex_array_size; uint8_t *hex_array_ptr = sl_cli_get_argument_hex(args, 3, &hex_array_size); // uint8_t ptr to {0xAA, 0xBB, 0xCC}, hex_array_size = 3 }
◆ sl_cli_get_argument_string
#define sl_cli_get_argument_string | ( | a, |
|
n |
|||
) | ((char *)(a->argv[a->arg_ofs + n])) |
Obtain string arguments.
- Parameters
-
[in] a
A pointer to the command arguments. [in] n
The argument number. The first argument is the number 0, the next 1, etc.
- Returns
- The argument value. For hex arguments, the return value is a pointer to a buffer containing decoded values. For string arguments, the return value is a pointer to the string.
An example could be the CLI input of example_sub_menu example_command hello 255 -100 {AA BB CC}
with corresponding C code of: void example_command(sl_cli_command_arg_t *args) { // Get the arguments (after the command strings). char *text_ptr = sl_cli_get_argument_string(args, 0); // char ptr to // "hello" uint8_t num1_u8 = sl_cli_get_argument_uint8(args, 1); // num1_u8 = 255 int16_t num2_i16 = sl_cli_get_argument_int16(args, 2); // num2_i16 = -100 size_t hex_array_size; uint8_t *hex_array_ptr = sl_cli_get_argument_hex(args, 3, &hex_array_size); // uint8_t ptr to {0xAA, 0xBB, 0xCC}, hex_array_size = 3 }
◆ sl_cli_get_command_count
#define sl_cli_get_command_count | ( | a | ) | ((int)(a->arg_ofs)) |
Obtain the number of command strings.
Users obtain the number of command strings with this macro.
- Parameters
-
[in] a
The number of command strings.
- Returns
- The number of command strings.
An example could be the CLI input of example_sub_menu example_command hello 255 -100 {AA BB CC}
with corresponding C code of: void example_command(sl_cli_command_arg_t *args) { // Get the number of command strings (before the arguments). int cmd_count = sl_cli_get_command_count(args); // cmd_count = 2 // (first string being "example_sub_menu" and second "example_command") }
◆ sl_cli_get_command_string
#define sl_cli_get_command_string | ( | a, |
|
n |
|||
) | ((char *)(a->argv[n])) |
Obtain the command string(s).
Users get the command string with this macro. If the command is used in a group, both the group string(s) and command string can be obtained. The total number of command strings is available in the command argument arg_ofs variable.
- Parameters
-
[in] a
A pointer to the command arguments. [in] n
The command string number. The first string is number 0, the next 1, etc.
An example could be the CLI input of example_sub_menu example_command hello 255 -100 {AA BB CC}
with corresponding C code of: void example_command(sl_cli_command_arg_t *args) { // Get the command strings (before the arguments). char *cmd1_ptr = sl_cli_get_command_string(args, 0); // char ptr to // "example_sub_menu" char *cmd2_ptr = sl_cli_get_command_string(args, 1); // char ptr to // "example_command" }
◆ SL_CLI_INPUT_DIRECTION_UP
#define SL_CLI_INPUT_DIRECTION_UP (1) |
MACROS ************************************.
Define the UP-direction.
◆ SL_CLI_INPUT_DIRECTION_DOWN
#define SL_CLI_INPUT_DIRECTION_DOWN (-1) |
Define the DOWN-direction.
◆ SL_CLI_ARG_UINT8
#define SL_CLI_ARG_UINT8 (0x00U) |
UINT8 argument type.
◆ SL_CLI_ARG_UINT16
#define SL_CLI_ARG_UINT16 (0x01U) |
UINT16 argument type.
◆ SL_CLI_ARG_UINT32
#define SL_CLI_ARG_UINT32 (0x02U) |
UINT32 argument type.
◆ SL_CLI_ARG_INT8
#define SL_CLI_ARG_INT8 (0x03U) |
INT8 argument type.
◆ SL_CLI_ARG_INT16
#define SL_CLI_ARG_INT16 (0x04U) |
INT16 argument type.
◆ SL_CLI_ARG_INT32
#define SL_CLI_ARG_INT32 (0x05U) |
INT32 argument type.
◆ SL_CLI_ARG_STRING
#define SL_CLI_ARG_STRING (0x06U) |
STRING argument type.
◆ SL_CLI_ARG_HEX
#define SL_CLI_ARG_HEX (0x07U) |
HEX argument type.
◆ SL_CLI_ARG_UINT8OPT
#define SL_CLI_ARG_UINT8OPT (0x10U) |
Optional UINT8 argument type.
◆ SL_CLI_ARG_UINT16OPT
#define SL_CLI_ARG_UINT16OPT (0x11U) |
Optional UINT16 argument type.
◆ SL_CLI_ARG_UINT32OPT
#define SL_CLI_ARG_UINT32OPT (0x12U) |
Optional UINT32 argument type.
◆ SL_CLI_ARG_INT8OPT
#define SL_CLI_ARG_INT8OPT (0x13U) |
Optional INT8 argument type.
◆ SL_CLI_ARG_INT16OPT
#define SL_CLI_ARG_INT16OPT (0x14U) |
Optional INT16 argument type.
◆ SL_CLI_ARG_INT32OPT
#define SL_CLI_ARG_INT32OPT (0x15U) |
Optional INT32 argument type.
◆ SL_CLI_ARG_STRINGOPT
#define SL_CLI_ARG_STRINGOPT (0x16U) |
Optional STRING argument type.
◆ SL_CLI_ARG_HEXOPT
#define SL_CLI_ARG_HEXOPT (0x17U) |
Optional HEX argument type.
◆ SL_CLI_ARG_ADDITIONAL
#define SL_CLI_ARG_ADDITIONAL (0x20U) |
ADDITIONAL argument type.
◆ SL_CLI_ARG_WILDCARD
#define SL_CLI_ARG_WILDCARD (0x21U) |
WILDCARD argument type.
◆ SL_CLI_ARG_GROUP
#define SL_CLI_ARG_GROUP (0xFEU) |
GROUP argument type.
◆ SL_CLI_ARG_END
#define SL_CLI_ARG_END (0xFFU) |
END argument type.
◆ SL_CLI_COMMAND
#define SL_CLI_COMMAND | ( | function, |
|
help_text, |
|||
arg_help, |
|||
... |
|||
) |
A macro, which is used to create commands.
◆ SL_CLI_COMMAND_GROUP
#define SL_CLI_COMMAND_GROUP | ( | group_table, |
|
help_text |
|||
) |
A macro, which is used to create command groups.
Variable Documentation
◆ sl_cli_default_handle
sl_cli_handle_t sl_cli_default_handle |
The default CLI handle.
◆ sl_cli_default_command_group
sl_cli_command_group_t* sl_cli_default_command_group |
The default CLI command group.