KEYSCAN

Description

Keyscan driver.

Data Structures

struct  sl_keyscan_driver_process_keyscan_event_handle_t
 

Functions

sl_status_t sl_keyscan_driver_init (void)
 Initializes the keyscan driver.
 
void sl_keyscan_driver_subscribe_event (sl_keyscan_driver_process_keyscan_event_handle_t *event_handle)
 Registers an event callback on Keyscan event.
 
void sl_keyscan_driver_unsubscribe_event (sl_keyscan_driver_process_keyscan_event_handle_t *event_handle)
 Unregisters an event callback on Keyscan event.
 
sl_status_t sl_keyscan_driver_start_scan (void)
 Starts the keyscan scan.
 
sl_status_t sl_keyscan_driver_stop_scan (void)
 Stops the keyscan scan.
 

Typedefs

typedef void(* sl_keyscan_driver_process_keyscan_event) (uint8_t *p_keyscan_matrix, sl_keyscan_driver_status_t status)
 

Enumerations

enum  sl_keyscan_driver_status_t {
  SL_KEYSCAN_STATUS_KEYPRESS_VALID = 0,
  SL_KEYSCAN_STATUS_KEYPRESS_INVALID,
  SL_KEYSCAN_STATUS_KEYPRESS_RELEASED
}
 KEYSCAN status values.
 

Function Documentation

◆ sl_keyscan_driver_init()

sl_status_t sl_keyscan_driver_init ( void  )

Initializes the keyscan driver.

◆ sl_keyscan_driver_subscribe_event()

void sl_keyscan_driver_subscribe_event ( sl_keyscan_driver_process_keyscan_event_handle_t event_handle)

Registers an event callback on Keyscan event.

◆ sl_keyscan_driver_unsubscribe_event()

void sl_keyscan_driver_unsubscribe_event ( sl_keyscan_driver_process_keyscan_event_handle_t event_handle)

Unregisters an event callback on Keyscan event.

◆ sl_keyscan_driver_start_scan()

sl_status_t sl_keyscan_driver_start_scan ( void  )

Starts the keyscan scan.

◆ sl_keyscan_driver_stop_scan()

sl_status_t sl_keyscan_driver_stop_scan ( void  )

Stops the keyscan scan.

Enumeration Type Documentation

◆ sl_keyscan_driver_status_t

KEYSCAN status values.