Legacy HAL

Description

Legacy HAL API.

Modules

Application Bootloader Interface
Definition of the application bootloader interface.
 
Common Bootloader
Common bootloader interface defines and functions.
 
Cyclic Redundancy Check
Functions that provide access to cyclic redundancy code (CRC) calculation. See crc.h for source code.
 
Diagnostics
Crash and watchdog diagnostic functions.
 
LED
Sample API funtions for controlling LEDs.
 
Microcontroller functions
Microcontroller functions.
 
Random Numbers
Functions that provide access to random numbers.
 
Reset Cause Definitions
Definitions for all the reset cause types.
 
SimEE2 to NVM3 Upgrade
 
Simulated EEPROM 1 and 2
Simulated EEPROM 1 and 2 legacy storage.
 
Standalone Bootloader
Definition of the standalone bootloader interface.
 

Functions

uint16_t halCommonGetInt16uMillisecondTick (void)
 
uint32_t halCommonGetInt32uMillisecondTick (void)
 
uint64_t halCommonGetInt64uMillisecondTick (void)
 
uint16_t halInternalStartSystemTimer (void)
 
void halCommonDelayMicroseconds (uint16_t us)
 
void halCommonDelayMilliseconds (uint16_t ms)
 
void halStackRadioPowerMainControl (bool powerUp)
 
void halStackRadioPowerUpBoard (void)
 
void halStackRadioPowerDownBoard (void)
 
void halStackProcessBootCount (void)
 
EmberStatus emDebugInit (void)
 
void emRadioSeedRandom (void)
 

Macros

#define simulatedTimePasses()